Hi,
I am trying to set up my 6657-EVM to work with Desktop-Linux-SDK,
I know that it is not directly supported but I am trying to port it in order to make it work and someone from TI told me that it was feasible.
I have the following problem though which is kind of blocking.
** I cannot get my 6657 listed with "lspci".
Is there something I must do special to get it ?
My dip switches are as follow:
Sw9 (1,2) : (OFF,ON)
Sw5 (1,2,3,4,5,6,7,8) : (ON,ON,ON,OFF,ON,ON,ON,ON)
Sw3 (1,2,3,4,5,6,7,8) : (OFF,ON,ON,OFF,ON,ON,ON,ON)
Thank you