Hello Engineers!
I am trying to execute WinCE on L138 LCDK board (195$) and i am not able to do this... :(
I do everything like it described here: http://processors.wiki.ti.com/index.php/AM18x/OMAP-L138_WinCE_BSP_Quick_Start_Guide (switches are different) and here: http://processors.wiki.ti.com/index.php/ARM9_WinCE_BSP_User_Guide#Flashing_EBOOT_to_OMAP-L138.2FAM18x_Development_Kit_.28NAND_Flash.29
I am using BSP_WINCE_ARM9_01_10_00.
I am trying to execute eBoot: ebootxxxflash from SD card, from NAND, but it is not working. I do not see any message on my hyperterminal.
I see BOOTME when switching to UART boot mode (SW 0101), and i am able to boot linux from NAND and SD with: u-boot-lcdk_ais.bin
But for some reason WinCE is not working. :(
Have someone the same problems or know someone solution?
Thanks and Respects,
Dmitry