I need to support 2 nand flash chip in my product.
I had modify GPMC_CONFIG7, but It can't work. Kernel will crash or hang.
CS0 GPMC_CONFIG7, is 0x48
Can anyone can help me to modify GPMC_CONFIG7 of CS1.
I know the GPMC_CONFIG7 BASEADDRESS define is "CSi base address where i = 0 to 3 (16 Mbytes minimum granularity). Bits [5-0] corresponds to A29, A28, A27, 26, 25, and A24."
But I can find out a right setting value.
Both of nand flash size is 256MB