This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO port control on C6678



Dear Sir.

I'm trying to make a simple SRIO repeater application using 6678EVM.
You know, 6678 has 4 SRIO ports and I want to read/write to different 1x port in my application.
That is, I want send data to lane0 or lane1 separately, and vice versa for recv logic.

I read user guide and found that I should control PLM_SP(n)_PATH_CTL register or CSL_SRIO_SetPLMPortPathControlMode funciton.

At this time, my question is how can I actually direct output port in SRIO LLD level when I use Srio_sockSend or Srio_sockRecv function.
SRIO LLD contains some control functions, but I cannot find any parameter for lane port control.

Regards,
Stellar

  • Are you using directIO traffic, or messaging?  I'll ask someone more familiar with the LLD to respond, but if it is directIO traffic and uses the LSU, there is a portID field in LSU_Reg4.  If you use messaging, the TX queue to output port mapping is done with the RIO_TX_QUEUE_SCH_INFOn registers.

    Regards,

    Travis

  • I use streaming (type9) data traffic in my program.

    And, I reviewed C:\ti\pdk_C6678_1_1_2_5\packages\ti\drv\srio\src\srio_drv.c code.

    For DIO, there is code for LSU_Reg4 handling in Srio_sockSend_DIO function.

    But I still cannot find code for messaging type9 packet.

    Is RIO_TX_QUEUE_SCH_INFOn register control is not included in srio_drv.c ?