This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone Black Sitara SDK 6.0

I've been successfully running Arago using tftp and SD card using serial port as console. Now I want to use HDMI and I am getting the following problem:

[    1.851257] omapfb omapfb: no displays
[    1.855224] omapfb omapfb: failed to setup omapfb
[    1.860168] omapfb: probe of omapfb failed with error -22

I configured supplied kernel 3.2 to use frame buffer and all displays and still nothing.

I tried using dts support and without dts.

I also tried gentoo and it works fine as it should.

Has anyone run it using HDMI output and if yes what configuration?

Mariusz