This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AUDIO: DEC -> AUDIO: Rpe process call failed, status: 1

Hi,

I am using DVR-RDK3.50 for DM8168 EVM.

I am trying to decode AAC audio frames coming from RTSP client. But Adec_process() funtion returns the error "AUDIO: DEC -> AUDIO: Rpe process call failed, status: 1"

See below code,

    memcpy((void *)b129AudDecCtrl.inBuf, pBuffer, bufferSize);

    b129AudDecCtrl.decPrm.inBuf.dataBufSize = bufferSize;
    b129AudDecCtrl.decPrm.inBuf.dataBuf = b129AudDecCtrl.inBuf;
    b129AudDecCtrl.decPrm.outBuf.dataBufSize = b129AudDecCtrl.outBufSize;
    if(Adec_process(b129AudDecCtrl.decHndl, &b129AudDecCtrl.decPrm) < 0)
    {
        printf("Failed to processd encoded audio\n");
        return -1;
    }

pBuffer here in this case is a buffer received from RTSP client and bufferSize is number of bytes that pBuffer contains.

can anyone tell which situation causes this error ?

Seeking quick response.

Shabbir Limdiwala