Hi,
I have a question about AM335x Linux SDK v6.00.
I understand that SDKv6.00 are base on Linaro Tool Chain.
My question is following:
In the directory ti-sdk-am335x-evm-06.00.00.00\filesystem,
there are two filesystem:
"arago-base-tisdk-image-am335x-evm.tar.gz"
"tisdk-rootfs-image-am335x-evm.tar.gz"
Is these two filesystem build with Linaro Tool Chain?
The first filesystem is named arago, so I thought it was build by arago Tool Chain.
By the way, does "tool chain" be used when building filesystem?
best regards,
g.f.