Hello,
I'd like to use System Analyzer to verify CPU load in realtime.
However it doesn't work. I checked http://processors.wiki.ti.com/images/b/bc/MCSA1.1_User_Guide.pdf - it must be simple:
1) I included "System Analyzer (UIA Target)" in Project->Properties->General->RTSC.
2) I added module "LoggingSetup" using UI tool (XGCONF). Manual tells all needed for me options must be configured by default (CPU Load).
3) a) However I changed to UploadMode_JTAGRUNMODE. But it didn't work for UploadMode_JTAGSTOPMODE too.
b) I have setup SYS/BIOS library type to "Custom" with Asserts and Logs set to OFF.
THEN, it is successfully built, when running app - System Analyzer Welcome screen and Menu Entries tell everything is OK, but I can't receive anything. No any data. Empty white graph windows forever.
Tries to play with manual options for "Load module", "LoggerCircBuff" - no any result.
What am I doing wrong?
I use:
CCS - 5.3.0.00090
SYS/BIOS - 6.34.2.18
System Analyzer (UIA Target) - 1.1.1.14
Windows 7 (English locale)
Target processor - C6748
-------------------------