This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678LE I2C EEPROM writer error on IBL



I'm trying to run the MCSDK video PKT demos,

The first part of this demo is to flash the board using IBL:

http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide#IBL

The board is no boot mode, when I run the script to flash script"EVM c6678 IBL" -> setConfig_c6678_main. I get the following error.

I have follow the instruction from the user guide 

Error:

[C66xx_0] EEPROM Writer Utility Version 01.00.00.04
[C66xx_0] 
[C66xx_0] Writing 51932 bytes from DSP memory address 0x80000000 to EEPROM bus address 0x0051 starting from device address 0x0000 ...
[C66xx_0] Returned platform error number is 4
[C66xx_0] EEPROM write failed


Thanks.