This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 / DDR3 Placement & Routing


Hi,


I am working on board layout based on DM8148 and was referring to layout guideline given in the datasheet for DDR3 placement and routing. Related to those guidelines I have one query related to DDR3 chip placement on board.


My question :


Which DDR3 chip should be placed near to processor? Lower data byte or higher data byte? Or it is irrespective which DDR3 chip is placed near to processor. Below snapshot from datasheet will clarify my question further.


 
Above snapshot is taken from DM8148 datasheet page 317 under section "8.13.4.2.4.15.2 DQS and DQ Routing Specification". This section is related to routing guideline of data and DQS signals. Above snapshot shows lower data byte DDR chip is placed far from the processor and highest data byte DDR chip is placed nearest to processor. I have shown the routing of clock, control and address bus with red line which denotes clock will be routed first to higher data byte DDR and last in lower data byte DDR. Is this placement and routing of DDR3 correct? Or it is irrespective which data byte DDR placed near to processor and which DDR placed far from processor?


Thanks,
M