Hello,
we are using IPNC RDK 3.5 and I'm trying to show a u-boot logo on the HDMI out.
I' ve got the recent u-boot source tree from here:
http://arago-project.org/git/projects/u-boot-ipnc-rdk-dm81xx.git,
configured (the second stage) with make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8148_ipnc_config_sd,
built it and the Mistral 8148 eval Board boots fine with it.
What do I have to do, to show a boot-logo on the HDMI output during u-boot start?
Thanks in advance!
Norbert