This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to serial programming omap-L137/AM1707 bootloader ?

Genius 5960 points
Other Parts Discussed in Thread: AM1707, OMAP-L137

Hi

I have tried the SPI boot of OMAPL137/AM1707 by reference to the following pages

http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L137

I have tried the SPI boot of OMAPL137/AM1707 by reference to the following pages

○ AM1707
  sfh_OMAP-L137.exe-targetType AM1707-flash ubl-spi.bin u-boot.bin-p COM60

○ OMAPL137
  sfh_OMAP-L137.exe-targetType OMAPL137_v1-baud 230400-flash_dsp dsp-spi-ais.bin ubl-spi.bin u-boot.bin-p COM60

We write to my SPI both without problems, u-boot does not start.

File you are using is using the files that are located in the following places.
C: \ OMAPL137_dsp_1_00_00_11 \ REL_LSP_02_20_00_07 \ PSP_02_20_00_07 \ bin

Please help someone.

Best Regards,

hamada