Other Parts Discussed in Thread: OMAPL138, TVP5147, TVP5146, OMAP-L138
Hi mates! I work under the project based on OMAPL-138(eXperimenter Kit from LogicPD). I have ADV7180 video ADC. It gets video from its CVBS input, converts it to digital format and sends it to OMAP(ARM Core) over VPIF capture input. After video processing on OMAP video signal has to be sent to video signal supplyers over external Wi-Fi interface. I use DaVinci-PSP-SDK-03.21.00.04 and linux kernel sources linux-03.21.00.04. I connected digital video signal lines from ADV7180 to VPIF_DIN and tryed to run it in the kernel. I turned on kernel options described in VPIF section as shown there: http://processors.wiki.ti.com/index.php/GSG:_Building_Software_Components_for_OMAP-L1#Driver_configuration_in_the_Linux_kernel , except turning on tvp514x, because i haven`t this chip, but I have ADV7180 chip and I turned it on. I also turned on Video4linux support and connected options v4l options. But after kernel compiling I haven`t v4l interface and there is no any devices like video input/output devices in /dev. Then I had turned on support tvp514x, and video0/video1 interfaces appeared in /dev. These interfaces are connected with tvp514x chip, but I haven`t this chip. There is also another problem: either tvp514x chip or ADV7180 chip are controlled over i2c bus. When I turn on tvp514x support in the kernel I get two addreses to control tvp514x in /sys/bus/i2c/ They are 5с and 5d in haxadecimal and 92/93 in decimal format. But ADV7180 has 42 address to read and 43 to write on i2c bus. And there is no adv7180 i2c control addresses in the system. So there is a question, how to make adv7180 work over VPIF with OMAP using i2c?