Other Parts Discussed in Thread: TMS320C6748
Hello I'm tring to run the clock example on my TMS320C6748 DSP.
(Code Composer Studio Version: 5.3.0.00090 , sys/bios 6.34.2.18)
When I run the code which creates 2 clock functions, non of which is reached, I can see the clock ticks are not increasing (in ROV view)
I also can the see the clocks are created, enabled and started (in ROV view)
What else should be configured for the clock to start working ?Do I need to configure the Timer module ? Do I need to Init the Power Module somehow ?
I'm not interested in using .gel files, what kind of initializations I need to do?
Thank you In advance
Alla