Hello,
Apologies if this is the wrong forum to post this in, but I can't find a NDK forum.
I'm using the DM648 with NDK2.0 and the http server to stream jpeg images to a web browser. The images are updated by javascript. The problem I'm having is that each cgi request is starting a new socket and I think task, when there is frequent polls from the browser the DM648 can't cope. I'm seeing lots of these errors:
00018.942 SBNew: Buffer OOM
Firstly is there a way to change the http server to use the same socket/task for each cgi request? I understand http1.0 is used in NDK2.0 and http1.1 supports persistent connections. Do more recent versions of NDK have http1.1?
Secondly, can I change to memory allocation to stop this error, and if so how?
Thanks Simon