This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LLC_mmcsdRead to unaligned memory



I'm using llc_mmcsd.c from biospsp 3.00.01.00 on a C6746, using a custom board. I need to read from SD card, and in some cases to an unaligned memory address. But then LLC_mmcsdRead fails, and reads into one, two or three bytes before my actual buffer.

I changed the code to:

    if ((Uint32)buf % sizeof(Uint32) == 0)
    {
        // Aligned buffer, fast read: 32 bits at a time
        Uint32* readBuf = (Uint32 *) buf;
        for (i = 0; i < (numBytes / FIFO_WIDTH_IN_BYTES); i++)
        {
            *readBuf = regs->MMCDRR;
            readBuf++;
        }
    }
    else
    {
        // Unaligned memory. Slow path: just 8 bits at a time
        Uint8* readBuf = (Uint8 *) buf;
        Uint32 val;
        for (i = 0; i < (numBytes / FIFO_WIDTH_IN_BYTES); i++)
        {
            val = regs->MMCDRR;
            *readBuf++ = (val >> 0) & 0xFF;
            *readBuf++ = (val >> 8) & 0xFF;
            *readBuf++ = (val >> 16) & 0xFF;
            *readBuf++ = (val >> 24) & 0xFF;
        }
    }

That works for me, but feels a bit ugly. Is there a better way? And in any case, I think the original code needs a patch.

Regards,

Michiel