This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DUAL ETHERNET

Dear All,

We are currently working on the customized board. In the customized board we have to DSP C6678 processors. There are totaly (8cores for DSP1 + 8cores for DSP2)

16 cores. In the customized board we have two ethernet port's. We are trying to enable ethernet port1 for core0 of DSP1 with a Seperate MAC Address and IP Address.

We are also trying to enable ethernet port2 for core1 of DSP1 with a Seperate MAC Address and IP Address.

When we try to port the helloworld_evmc6678l.out file for core 0  the output is

[C66xx_0] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized

TCP/IP Stack 'Hello World!' Application


TCP/IP Stack 'Hello World!' Application

PASS successfully initialized
Init_Cpsw: Configure MAC- 00-17-EA-CD-CE-2D
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC    : Enabled  :          : 000
Service Status: DHCPC    : Enabled  : Running  : 000
Network Added: If-1:172.17.2.17
Service Status: DHCPC    : Enabled  : Running  : 017

When i Change the Init_SGMII(1) to Init_SGMII(0) in platform_lib_evmc6678l/platform.c and i compiled the files and i ported the helloworld_evmc6678l.out to core 1 the output is

[C66xx_1] Error: Inserting memory region 0, Error code : -135
Failed to initialize the QMSS subsystem

   0:48              0:96              0:128             0:256          
   0:512             0:1536            0:3072         
(0/0 mmAlloc: 0/0/0, mmBulk: 0/0/0)

And i came to know that whether any changes has to be done in .cfg file to clear the error.

Regards,

Avinash N