Now the board can boot up with the nand flash,then i want flashing a new xload image into the flash from uboot command.but it can't work.here is my steps:
1. Make a x-load.bin image in ubuntu,just add some printf() function to indicate the change.
2. Signing the image by signGP tools into x-load.bin.fit.
3. Download the image to ddr memory in certen area,erase the flash,write flash,all complished with success.of cause,flashing area is 0x0~0x80000.
4. Re-Power the board,it can't work.
what's wrong?
I compared x-load.bin with x-load.bin.fit,which is signGP's product,they only have a bit different in the head of file by 8bytes.see the picture.Is the difference is right? I mean the translated file by signGP tool is right??