This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to support OMAPL138 on DSPLink 1.62

Other Parts Discussed in Thread: OMAPL138, OMAP-L138, DA8XX, OMAP3530

Questions:

dsplink_1_62_02 ( from TI ) can't be configured as OMAPL138 platform.  How to support it? Is it easy?

>dsplinkcfg.bat

****************** ERROR !!! ***************************
Please provide a valid Platform!
Following platform are supported currently:
ID-->JACINTO1
Jacinto SoC version 1 - C64P DSP interfaced directly to ARM9
This platform can connect to a DM6437 device via VLYNQ
ID-->JACINTO2
Jacinto SoC Version 2 - C64P DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->DRX45X
DRX45X SoC version 1 - C64P DSP interfaced directly to ARM9
This platform can connect to a DM6437 device via VLYNQ
Provided:
Example: --platform=DAVINCI or --platform=<ID> or --help for all options

Background

I'm running QNX on ARM core on OMAPL138 platform. And QNX only provide DSPLink 1.62 package.  

BuildNumber = 20110191038
PatchNum = 2275
Name = DSPLINK-162
Baseline = 640

In this package, it doesn't include any DSP side code.  So I downloaded the version. 1.62.02 to build, with not support error above.

Thanks,

Fuquan