We got reports of a couple of ( >10) our devices in the field not working any more, only a power cycle helped.
With the scope I found the cpu was totally dead, no GPIO pins where toggling (could not measure the DDR ram signals) and no clocks.
On the second device the same thing again but now I got deeper into the clock signal and could measure a very weak 26MHz on the XTAL (120mV).
Could it be that these device are in DeepSleep mode ?
We are using Windows Compact 7 and don't use any sleep modes in the application.
Any way I can check or prevent Windows CE7 to go into any sleep functions ?