Hi all
I have some questions about dm8168 dvrrdk link application
1. can scale link do up load scale and crop the out side image?
In my application, i want to up scale 1024x768(center 512x384) image x2, and crop 1024x786 to display,
i know display link can zoom and set zoom center position dynamically, however osd also scaled and run out display area ,
so i want to know if i scale link can do this, as there is no interface to set zoom center position dynamically or how to do this?
2.Can menu drawn by graph link can be encoded together with video frame?
I see the graph link which can draw osd also, so i want to use it to draw menu but when encode video frame will the osd is overlay the frame?
How can i do this ?
best regards
xavier