Other Parts Discussed in Thread: SYSCONFIG, ADS7846
Hi All,
we have configured EHCI for ULPI - 12pin - port2. We have a PHY SMSC3320 connected to this. There is an external hub connected to the PHY. We are curently using 2.6.27 kernel. But i have back ported the latest EHCI related patches from 2.6.32-rc8.
During boot up, I cannot see that our external hub getting enumerated. Instead i get either of the below two messages in different boots.
1. hub 1-0:1.0: port 2 not reset yet, waiting 200ms....... hub 1-0:1.0: Cannot enable port 2. Maybe the USB cable is bad?
2. hub 1-0:1.0: unable to enumerate USB device on port 2
Our PHY takes 60 MHZ clock input and we can probe the same. I have pasted the logs which i am getting(sorry, its with all debug messages enabled).[I am sorry i couldnt see any attachment option for the port]
1. How do i ensure that our PHY is working?
2. I have taken ehci-omap.c completely and ported ehci related changes in board-omap3evm.c from 2.6.32-rc8. Is there any relavant ehci related code to be ported?
It will be really great if anybody can help me on this.
Thanks & Regards,
-- Srinivas R
------------------------------------------------------------Boot logs start ------------------------------------------------------------------------------------------------------------------------------------
U-Boot 2008.10 (Nov 25 2009 - 15:15:17)
U-Boot code: 80E80000 -> 80EA7ACC BSS: -> 80EDD7F8
OMAP35X-Family-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3 NGT board + LPDDR/NOR FLASH
In: serial
Out: serial
Err: serial
Changes added for MMC boot
### main_loop entered: bootdelay=5
### main_loop: bootcmd="mmcinit;fatload mmc 0 0x80000000 uImage;bootm 80000000"
Hit any key to stop autoboot: 0
reading uImage
FAT32, fatlength: 618
Rootdir begins at sector: 1272, offset: 9f000, size: 1
Data begins at: 1270
Cluster size: 1
Rootvfatname: ||
RootMismatch: |fat||
RootMismatch: |mlo||
Rootvfatname: |uimage|
RootName: uimage, start: 0xc234, size: 0x26c850
Filesize: 2541648 bytes
Reading: 2541648 bytes
gc - clustnum: 49716, startsect: 50986
gc - clustnum: 54680, startsect: 55950
Size: 2541648, got: 2541648
2541648 bytes read
* kernel: cmdline image address = 0x80000000
## Booting kernel from Legacy Image at 80000000 ...
Image Name: Linux-2.6.27.18
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2541584 Bytes = 2.4 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
kernel data at 0x80000040, len = 0x0026c810 (2541584)
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
Loading Kernel Image ... OK
OK
kernel loaded at 0x80008000, end = 0x80274810
images.os.start = 0x80000000, images.os.end = 0x8026c850
images.os.load = 0x80008000, load_end = 0x80274810
## Transferring control to Linux (at address 80008000) ...
Starting kernel ...
Uncompressing Linux..........................................................................................................................................
<5>Linux version 2.6.27.18 (srinivas@srinivas-desktop) (gcc version 4.2.1 (CodeSourcery Sourcery G++ Lite 2007q3-51)) #80 Sun Dec 13 17:17:36 IST 2009
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=00c5387f
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
<7>On node 0 totalpages: 131072
<7>free_area_init_node: node 0, pgdat c046183c, node_mem_map c04b3000
<7> DMA zone: 130048 pages, LIFO batch:31
<6>start of evm map io
<4>BUG: mapping for 0x48000000 at 0xd8000000 overlaps vmalloc space
<4>BUG: mapping for 0x48300000 at 0xd8300000 overlaps vmalloc space
<4>BUG: mapping for 0x49000000 at 0xd9000000 overlaps vmalloc space
<4>BUG: mapping for 0x54000000 at 0xe4000000 overlaps vmalloc space
<6>OMAP3430 ES3.1
<6>SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
<6>end of evm map io
CPU0: L1 I VIPT cache. Caches unified at level 2, coherent at level 3
CPU0: Level 1 cache is separate instruction and data
CPU0: I cache: 16384 bytes, associativity 4, 64 byte lines, 64 sets,
supports RA
CPU0: D cache: 16384 bytes, associativity 4, 64 byte lines, 64 sets,
supports RA WB WT
CPU0: Level 2 cache is unified
CPU0: unified cache: 262144 bytes, associativity 8, 64 byte lines, 512 sets,
supports WA RA WB WT
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
<5>Kernel command line: console=ttyS2,115200n8 noinitrd root=/dev/mmcblk0p2 rw rootfstype=ext3
<6>start of evm irq init
<6>[SRI] start of omap2_clk_init
<6>[SRI] YES, cpu_is_omap34xx
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>[SRI] start of omap3_clkoutx2_recalc
<6>[SRI] end of omap3_clkoutx2_recalc
<6>Clocking rate (Crystal/DPLL/ARM core): 26.0/332/500 MHz
<6>[SRI] start of omap3_clk_lock_dpll5
<6>[SRI] start of omap3_noncore_dpll_set_rate
<6>[SRI] start of _omap3_dpll_compute_freqsel
<6>[SRI] end of _omap3_dpll_compute_freqsel
<6>[SRI] start of omap3_noncore_dpll_program
<6>[SRI] start of _omap3_noncore_dpll_bypass
<6>[SRI] start of _omap3_noncore_dpll_lock
<6>[SRI] start of omap3_dpll_autoidle_read
<6>[SRI] end of omap3_dpll_autoidle_read
<6>[SRI] start of _omap3_dpll_write_clken
<6>[SRI] End of _omap3_dpll_write_clken
<6>[SRI] start of _omap3_wait_dpll_status
<6>[SRI] end of _omap3_wait_dpll_status
<6>[SRI] start of map3_dpll_deny_idle
<6>[SRI] end of map3_dpll_deny_idle
<6>[SRI] end of _omap3_noncore_dpll_lock
<6>[SRI] end of omap3_noncore_dpll_program
<6>[SRI] end of omap3_noncore_dpll_set_rate
<6>[SRI] start of omap3_noncore_dpll_enable
<6>[SRI] start of _omap3_noncore_dpll_lock
<6>[SRI] start of omap3_dpll_autoidle_read
<6>[SRI] end of omap3_dpll_autoidle_read
<6>[SRI] start of _omap3_dpll_write_clken
<6>[SRI] End of _omap3_dpll_write_clken
<6>[SRI] start of _omap3_wait_dpll_status
<6>[SRI] end of _omap3_wait_dpll_status
<6>[SRI] start of map3_dpll_deny_idle
<6>[SRI] end of map3_dpll_deny_idle
<6>[SRI] end of _omap3_noncore_dpll_lock
<6>[SRI] end of omap3_noncore_dpll_enable
<6>[SRI] start of omap3_dpll_allow_idle
<6>[SRI] end of omap3_dpll_allow_idle
<6>[SRI] start of omap3_noncore_dpll_disable
<6>[SRI] start of _omap3_noncore_dpll_stop
<6>[SRI] start of omap3_dpll_autoidle_read
<6>[SRI] end of omap3_dpll_autoidle_read
<6>[SRI] start of _omap3_dpll_write_clken
<6>[SRI] End of _omap3_dpll_write_clken
<6>[SRI] start of omap3_dpll_allow_idle
<6>[SRI] end of omap3_dpll_allow_idle
<6>[SRI] start of _omap3_noncore_dpll_stop
<6>[SRI] start of omap3_noncore_dpll_disable
<6>[SRI] end of omap3_clk_lock_dpll5
<6>[SRI] end of omap2_clk_init
<6>GPMC revision 5.0
<6>IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
<6>Total of 96 interrupts on 1 active controller
<6>OMAP34xx GPIO hardware version 2.5
<6>end of evm irq init
PID hash table entries: 2048 (order: 11, 8192 bytes)
<6>[SRI] start of timer init
<6>OMAP clockevent source: GPTIMER1 at 32768 Hz
<6>hwtimer: Added OMAP2 timer (TI_OMAP2430SDP GP timer 3) at index=0
<6>[SRI] end of timer init
Console: colour dummy device 80x30
<6>Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
<6>Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
<6>Memory: 256MB 256MB = 512MB total
<5>Memory: 514816KB available (3492K code, 513K data, 756K init)
<6>Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
<6>CPU: Testing write buffer coherency: ok
<6>ftrace: allocating 11524 entries in 46 pages
<7>device: 'platform': device_add
<7>PM: Adding info for No Bus:platform
<7>bus: 'platform': registered
<7>Registering sysdev class 'cpu'
<6>net_namespace: 288 bytes
<6>NET: Registered protocol family 16
<7>device class 'bdi': registering
<7>device class 'tty': registering
<7>device class 'vtconsole': registering
<7>device: 'vtcon0': device_add
<7>PM: Adding info for No Bus:vtcon0
<7>bus: 'i2c': registered
<7>device class 'i2c-adapter': registering
<7>bus: 'i2c': add driver dummy
<3>[SRI] bus 1 registration start
<7>Registering platform device 'i2c_omap.1'. Parent at platform
<7>device: 'i2c_omap.1': device_add
<7>bus: 'platform': add device i2c_omap.1
<7>PM: Adding info for platform:i2c_omap.1
<3>[SRI] bus 2 registration start
<3>[SRI] bus 2 -- so set the base addr
<7>Registering platform device 'i2c_omap.2'. Parent at platform
<7>device: 'i2c_omap.2': device_add
<7>bus: 'platform': add device i2c_omap.2
<7>PM: Adding info for platform:i2c_omap.2
<7>Registering platform device 'i2c_omap.3'. Parent at platform
<7>device: 'i2c_omap.3': device_add
<7>bus: 'platform': add device i2c_omap.3
<7>PM: Adding info for platform:i2c_omap.3
<7>Registering platform device 'omap3evm_lcd'. Parent at platform
<7>device: 'omap3evm_lcd': device_add
<7>bus: 'platform': add device omap3evm_lcd
<7>PM: Adding info for platform:omap3evm_lcd
<7>Registering platform device 'smc911x'. Parent at platform
<7>device: 'smc911x': device_add
<7>bus: 'platform': add device smc911x
<7>PM: Adding info for platform:smc911x
<3>Serial init start
<6>[SRI] start of omap3_noncore_dpll_enable
<6>[SRI] start of _omap3_noncore_dpll_lock
<6>[SRI] start of omap3_dpll_autoidle_read
<6>[SRI] end of omap3_dpll_autoidle_read
<6>[SRI] start of _omap3_dpll_write_clken
<6>[SRI] End of _omap3_dpll_write_clken
<6>[SRI] start of _omap3_wait_dpll_status
<6>[SRI] end of _omap3_wait_dpll_status
<6>[SRI] start of map3_dpll_deny_idle
<6>[SRI] end of map3_dpll_deny_idle
<6>[SRI] end of _omap3_noncore_dpll_lock
<6>[SRI] end of omap3_noncore_dpll_enable
<3>Serial init end
<6>[SRI] configuring GPIO21 for PHY reset
<4>MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
<6>start of hsmmc init
<7>Registering platform device 'mmci-omap.0'. Parent at platform
<7>device: 'mmci-omap.0': device_add
<7>bus: 'platform': add device mmci-omap.0
<7>PM: Adding info for platform:mmci-omap.0
<6>end of hsmmc init
<6>start of musb init
<7>Registering platform device 'musb_hdrc'. Parent at platform
<7>device: 'musb_hdrc': device_add
<7>bus: 'platform': add device musb_hdrc
<7>PM: Adding info for platform:musb_hdrc
<6>end of musb init
<6>[SRI] SETTING THE EHCI MUX...
<6>[SRI] configuring port 1 for PHY mode
<4>MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
<4>MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
<4>MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
<4>MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
<4>MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
<4>MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
<4>MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
<4>MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
<4>MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
<4>MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
<4>MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
<4>MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
<7>Registering platform device 'ehci-omap.0'. Parent at platform
<7>device: 'ehci-omap.0': device_add
<7>bus: 'platform': add device ehci-omap.0
<7>PM: Adding info for platform:ehci-omap.0
<7>Registering platform device 'omap2_mcspi.1'. Parent at platform
<7>device: 'omap2_mcspi.1': device_add
<7>bus: 'platform': add device omap2_mcspi.1
<7>PM: Adding info for platform:omap2_mcspi.1
<7>Registering platform device 'omap2_mcspi.2'. Parent at platform
<7>device: 'omap2_mcspi.2': device_add
<7>bus: 'platform': add device omap2_mcspi.2
<7>PM: Adding info for platform:omap2_mcspi.2
<7>Registering platform device 'omap2_mcspi.3'. Parent at platform
<7>device: 'omap2_mcspi.3': device_add
<7>bus: 'platform': add device omap2_mcspi.3
<7>PM: Adding info for platform:omap2_mcspi.3
<7>Registering platform device 'omap2_mcspi.4'. Parent at platform
<7>device: 'omap2_mcspi.4': device_add
<7>bus: 'platform': add device omap2_mcspi.4
<7>PM: Adding info for platform:omap2_mcspi.4
<7>Registering platform device 'serial8250.0'. Parent at platform
<7>device: 'serial8250.0': device_add
<7>bus: 'platform': add device serial8250.0
<7>PM: Adding info for platform:serial8250.0
<6>[SRI] start of omap2_clk_arch_init
<7>Registering platform device 'omap_wdt'. Parent at platform
<7>device: 'omap_wdt': device_add
<7>bus: 'platform': add device omap_wdt
<7>PM: Adding info for platform:omap_wdt
<6>OMAP DMA hardware revision 4.0
<7>Registering sysdev class 'gpio'
<7>Registering sys device of class 'gpio'
<7>Registering sys device 'gpio0'
<7>Registering platform device 'omapfb'. Parent at platform
<7>device: 'omapfb': device_add
<7>bus: 'platform': add device omapfb
<7>PM: Adding info for platform:omapfb
<7>Registering sys device of class 'cpu'
<7>Registering sys device 'cpu0'
<3>USB: No board-specific platform config found
<3>Unable to set the DSSfunctional clock to 432000000
<6>OMAP Display hardware version 2.0
<7>device: 'default': device_add
<7>PM: Adding info for No Bus:default
<7>device class 'block': registering
<7>bus: 'platform': add driver twl4030_gpio
<7>device class 'graphics': registering
<7>device class 'misc': registering
<7>bus: 'i2c': add driver twl4030
<7>bus: 'platform': add driver i2c_omap
<7>bus: 'platform': driver_probe_device: matched device i2c_omap.1 with driver i2c_omap
<7>bus: 'platform': really_probe: probing driver i2c_omap with device i2c_omap.1
<6>physical address start :0x48070000 end:0x4807003f <6>mapped to :0xd8070000 <6>i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
<7>device: 'i2c-1': device_add
<7>PM: Adding info for No Bus:i2c-1
<7>device: '1-0048': device_add
<7>bus: 'i2c': add device 1-0048
<7>PM: Adding info for i2c:1-0048
<7>bus: 'i2c': driver_probe_device: matched device 1-0048 with driver twl4030
<7>bus: 'i2c': really_probe: probing driver twl4030 with device 1-0048
<7>device: '1-0049': device_add
<7>bus: 'i2c': add device 1-0049
<7>PM: Adding info for i2c:1-0049
<7>bus: 'i2c': driver_probe_device: matched device 1-0049 with driver dummy
<7>bus: 'i2c': really_probe: probing driver dummy with device 1-0049
<7>driver: '1-0049': driver_bound: bound to device 'dummy'
<7>bus: 'i2c': really_probe: bound device 1-0049 to driver dummy
<7>device: '1-004a': device_add
<7>bus: 'i2c': add device 1-004a
<7>PM: Adding info for i2c:1-004a
<7>bus: 'i2c': driver_probe_device: matched device 1-004a with driver dummy
<7>bus: 'i2c': really_probe: probing driver dummy with device 1-004a
<7>driver: '1-004a': driver_bound: bound to device 'dummy'
<7>bus: 'i2c': really_probe: bound device 1-004a to driver dummy
<7>device: '1-004b': device_add
<7>bus: 'i2c': add device 1-004b
<7>PM: Adding info for i2c:1-004b
<7>bus: 'i2c': driver_probe_device: matched device 1-004b with driver dummy
<7>bus: 'i2c': really_probe: probing driver dummy with device 1-004b
<7>driver: '1-004b': driver_bound: bound to device 'dummy'
<7>bus: 'i2c': really_probe: bound device 1-004b to driver dummy
<6>twl4030: PIH (irq 7) chaining IRQs 368..375
<6>twl4030: power (irq 373) chaining IRQs 376..383
<7>Registering platform device 'twl4030_gpio'. Parent at 1-0049
<7>device: 'twl4030_gpio': device_add
<7>bus: 'platform': add device twl4030_gpio
<7>PM: Adding info for platform:twl4030_gpio
<7>bus: 'platform': driver_probe_device: matched device twl4030_gpio with driver twl4030_gpio
<7>bus: 'platform': really_probe: probing driver twl4030_gpio with device twl4030_gpio
<6>twl4030: gpio (irq 368) chaining IRQs 384..401
<7>driver: 'twl4030_gpio': driver_bound: bound to device 'twl4030_gpio'
<7>bus: 'platform': really_probe: bound device twl4030_gpio to driver twl4030_gpio
<7>Registering platform device 'twl4030_keypad'. Parent at 1-004a
<7>device: 'twl4030_keypad': device_add
<7>bus: 'platform': add device twl4030_keypad
<7>PM: Adding info for platform:twl4030_keypad
<7>Registering platform device 'twl4030_usb'. Parent at 1-0048
<7>device: 'twl4030_usb': device_add
<7>bus: 'platform': add device twl4030_usb
<7>PM: Adding info for platform:twl4030_usb
<7>driver: '1-0048': driver_bound: bound to device 'twl4030'
<7>bus: 'i2c': really_probe: bound device 1-0048 to driver twl4030
<7>driver: 'i2c_omap.1': driver_bound: bound to device 'i2c_omap'
<7>bus: 'platform': really_probe: bound device i2c_omap.1 to driver i2c_omap
<7>bus: 'platform': driver_probe_device: matched device i2c_omap.2 with driver i2c_omap
<7>bus: 'platform': really_probe: probing driver i2c_omap with device i2c_omap.2
<6>physical address start :0x48072000 end:0x4807203f <6>mapped to :0xd8072000 <6>i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
<7>device: 'i2c-2': device_add
<7>PM: Adding info for No Bus:i2c-2
<7>device: '2-00a0': device_add
<7>bus: 'i2c': add device 2-00a0
<7>PM: Adding info for i2c:2-00a0
<7>driver: 'i2c_omap.2': driver_bound: bound to device 'i2c_omap'
<7>bus: 'platform': really_probe: bound device i2c_omap.2 to driver i2c_omap
<7>bus: 'platform': driver_probe_device: matched device i2c_omap.3 with driver i2c_omap
<7>bus: 'platform': really_probe: probing driver i2c_omap with device i2c_omap.3
<6>physical address start :0x48060000 end:0x4806003f <6>mapped to :0xd8060000 <6>i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
<7>device: 'i2c-3': device_add
<7>PM: Adding info for No Bus:i2c-3
<7>driver: 'i2c_omap.3': driver_bound: bound to device 'i2c_omap'
<7>bus: 'platform': really_probe: bound device i2c_omap.3 to driver i2c_omap
<7>bus: 'platform': add driver twl4030_usb
<7>bus: 'platform': driver_probe_device: matched device twl4030_usb with driver twl4030_usb
<7>bus: 'platform': really_probe: probing driver twl4030_usb with device twl4030_usb
<6>[SRI] start of twl4030_usb_probe
<6>twl4030_usb twl4030_usb: Initialized TWL4030 USB module
<6>[SRI] end of twl4030_usb_probe
<7>driver: 'twl4030_usb': driver_bound: bound to device 'twl4030_usb'
<7>bus: 'platform': really_probe: bound device twl4030_usb to driver twl4030_usb
<7>device class 'scsi_host': registering
<7>bus: 'scsi': registered
<7>device class 'scsi_device': registering
<5>SCSI subsystem initialized
<7>bus: 'spi': registered
<7>device class 'spi_master': registering
<7>bus: 'platform': add driver omap2_mcspi
<7>bus: 'platform': driver_probe_device: matched device omap2_mcspi.1 with driver omap2_mcspi
<7>bus: 'platform': really_probe: probing driver omap2_mcspi with device omap2_mcspi.1
<7>device: 'spi1': device_add
<7>PM: Adding info for No Bus:spi1
<7>device: 'spi1.0': device_add
<7>bus: 'spi': add device spi1.0
<7>PM: Adding info for spi:spi1.0
<7>driver: 'omap2_mcspi.1': driver_bound: bound to device 'omap2_mcspi'
<7>bus: 'platform': really_probe: bound device omap2_mcspi.1 to driver omap2_mcspi
<7>bus: 'platform': driver_probe_device: matched device omap2_mcspi.2 with driver omap2_mcspi
<7>bus: 'platform': really_probe: probing driver omap2_mcspi with device omap2_mcspi.2
<7>device: 'spi2': device_add
<7>PM: Adding info for No Bus:spi2
<7>driver: 'omap2_mcspi.2': driver_bound: bound to device 'omap2_mcspi'
<7>bus: 'platform': really_probe: bound device omap2_mcspi.2 to driver omap2_mcspi
<7>bus: 'platform': driver_probe_device: matched device omap2_mcspi.3 with driver omap2_mcspi
<7>bus: 'platform': really_probe: probing driver omap2_mcspi with device omap2_mcspi.3
<7>device: 'spi3': device_add
<7>PM: Adding info for No Bus:spi3
<7>driver: 'omap2_mcspi.3': driver_bound: bound to device 'omap2_mcspi'
<7>bus: 'platform': really_probe: bound device omap2_mcspi.3 to driver omap2_mcspi
<7>bus: 'platform': driver_probe_device: matched device omap2_mcspi.4 with driver omap2_mcspi
<7>bus: 'platform': really_probe: probing driver omap2_mcspi with device omap2_mcspi.4
<7>device: 'spi4': device_add
<7>PM: Adding info for No Bus:spi4
<7>driver: 'omap2_mcspi.4': driver_bound: bound to device 'omap2_mcspi'
<7>bus: 'platform': really_probe: bound device omap2_mcspi.4 to driver omap2_mcspi
<7>bus: 'usb': registered
<7>device class 'usb_host': registering
<7>bus: 'usb': add driver usbfs
<6>usbcore: registered new interface driver usbfs
<7>bus: 'usb': add driver hub
<6>usbcore: registered new interface driver hub
<7>bus: 'usb': add driver usb
<6>usbcore: registered new device driver usb
<6>musb_hdrc: version 6.0, musb-dma, otg (peripheral+host), debug=0
<7>bus: 'platform': add driver musb_hdrc
<7>bus: 'platform': driver_probe_device: matched device musb_hdrc with driver musb_hdrc
<7>bus: 'platform': really_probe: probing driver musb_hdrc with device musb_hdrc
<7>HS USB OTG: revision 0x33, sysconfig 0x2011, sysstatus 0x1, intrfsel 0x1, simenable 0x0
<7>musb_hdrc: ConfigData=0x55 (UTMI-16, dyn FIFOs, bulk split (X), HB-ISO Rx (X))
<7>musb_hdrc: MHDRC RTL version 1.400
<7>musb_hdrc: setup fifo_mode 4
<7>musb_hdrc: 29/31 max ep, 15424/16384 memory
<7>musb_hdrc: hw_ep 0shared, max 64
<7>musb_hdrc: hw_ep 1tx, max 512
<7>musb_hdrc: hw_ep 1rx, max 512
<7>musb_hdrc: hw_ep 2tx, max 512
<7>musb_hdrc: hw_ep 2rx, max 512
<7>musb_hdrc: hw_ep 3tx, max 512
<7>musb_hdrc: hw_ep 3rx, max 512
<7>musb_hdrc: hw_ep 4tx, max 512
<7>musb_hdrc: hw_ep 4rx, max 512
<7>musb_hdrc: hw_ep 5tx, max 512
<7>musb_hdrc: hw_ep 5rx, max 512
<7>musb_hdrc: hw_ep 6tx, max 512
<7>musb_hdrc: hw_ep 6rx, max 512
<7>musb_hdrc: hw_ep 7tx, max 512
<7>musb_hdrc: hw_ep 7rx, max 512
<7>musb_hdrc: hw_ep 8tx, max 512
<7>musb_hdrc: hw_ep 8rx, max 512
<7>musb_hdrc: hw_ep 9tx, max 512
<7>musb_hdrc: hw_ep 9rx, max 512
<7>musb_hdrc: hw_ep 10tx, max 512
<7>musb_hdrc: hw_ep 10rx, max 512
<7>musb_hdrc: hw_ep 11tx, max 512
<7>musb_hdrc: hw_ep 11rx, max 512
<7>musb_hdrc: hw_ep 12tx, max 512
<7>musb_hdrc: hw_ep 12rx, max 512
<7>musb_hdrc: hw_ep 13tx, max 512
<7>musb_hdrc: hw_ep 13rx, max 512
<7>musb_hdrc: hw_ep 14shared, max 1024
<7>musb_hdrc: hw_ep 15shared, max 1024
<6>musb_hdrc: USB OTG mode controller at d80ab000 using DMA, IRQ 92
<7>device: 'gadget': device_add
<7>PM: Adding info for No Bus:gadget
<7>driver: 'musb_hdrc': driver_bound: bound to device 'musb_hdrc'
<7>bus: 'platform': really_probe: bound device musb_hdrc to driver musb_hdrc
<7>device class 'input': registering
<7>bus: 'mmc': registered
<7>device class 'mmc_host': registering
<7>bus: 'sdio': registered
<7>device class 'net': registering
<6>tracer: 898 pages allocated for 65536 entries of 56 bytes
<6> actual entries 65554
<7>Switched to high resolution mode on CPU 0
<7>device class 'mem': registering
<7>device: 'mem': device_add
<7>PM: Adding info for No Bus:mem
<7>device: 'kmem': device_add
<7>PM: Adding info for No Bus:kmem
<7>device: 'null': device_add
<7>PM: Adding info for No Bus:null
<7>device: 'zero': device_add
<7>PM: Adding info for No Bus:zero
<7>device: 'full': device_add
<7>PM: Adding info for No Bus:full
<7>device: 'random': device_add
<7>PM: Adding info for No Bus:random
<7>device: 'urandom': device_add
<7>PM: Adding info for No Bus:urandom
<7>device: 'kmsg': device_add
<7>PM: Adding info for No Bus:kmsg
<7>device: 'lo': device_add
<7>PM: Adding info for No Bus:lo
<6>NET: Registered protocol family 2
<6>IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
<6>TCP established hash table entries: 65536 (order: 7, 524288 bytes)
<6>TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
<6>TCP: Hash tables configured (established 65536 bind 65536)
<6>TCP reno registered
<6>NET: Registered protocol family 1
<7>Registering sysdev class 'timer'
<7>Registering sys device of class 'timer'
<7>Registering sys device 'timer0'
<4>NetWinder Floating Point Emulator V0.97 (double precision)
<7>Registering sysdev class 'timekeeping'
<7>Registering sys device of class 'timekeeping'
<7>Registering sys device 'timekeeping0'
<7>Registering sysdev class 'clocksource'
<7>Registering sys device of class 'clocksource'
<7>Registering sys device 'clocksource0'
<7>Synthetic TSC timer will fire each 131069 jiffies.
<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
<6>JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
<6>msgmni has been set to 1005
<6>io scheduler noop registered
<6>io scheduler anticipatory registered (default)
<6>io scheduler deadline registered
<6>io scheduler cfq registered
<6>LTT : ltt-relay init
<6>LTT : ltt-ftrace init
<6>[SRI] start of omapfb_init
<7>bus: 'platform': add driver omapfb
<7>bus: 'platform': driver_probe_device: matched device omapfb with driver omapfb
<7>bus: 'platform': really_probe: probing driver omapfb with device omapfb
<7>driver: 'omapfb': driver_bound: bound to device 'omapfb'
<7>bus: 'platform': really_probe: bound device omapfb to driver omapfb
<6>[SRI] end of omapfb_init
<6>[SRI] In omap3evm_panel_drv_init
<7>bus: 'platform': add driver omap3evm_lcd
<7>bus: 'platform': driver_probe_device: matched device omap3evm_lcd with driver omap3evm_lcd
<7>bus: 'platform': really_probe: probing driver omap3evm_lcd with device omap3evm_lcd
<6>[SRI] probing omap3evm_panel_probe
<6>omapfb: configured for panel omap3evm
<6>[SRI] start of omap_dispc_init
<6>omapfb: DISPC version 3.0 initialized
<6>[SRI] end of omap_dispc_init
<6>[SRI] In omap3evm_panel_enable
<7>device: 'fb0': device_add
<7>PM: Adding info for No Bus:fb0
<6>omapfb: Framebuffer initialized. Total vram 770048 planes 1
<6>omapfb: Pixclock 33230 kHz hfreq 29.9 kHz vfreq 57.2 Hz
<6>[SRI] registered omap3evm_panel
<7>driver: 'omap3evm_lcd': driver_bound: bound to device 'omap3evm_lcd'
<7>bus: 'platform': really_probe: bound device omap3evm_lcd to driver omap3evm_lcd
<7>device: 'tty': device_add
<7>PM: Adding info for No Bus:tty
<7>device: 'console': device_add
<7>PM: Adding info for No Bus:console
<7>device: 'ptmx': device_add
<7>PM: Adding info for No Bus:ptmx
<7>device: 'tty0': device_add
<7>PM: Adding info for No Bus:tty0
<7>device class 'vc': registering
<7>device: 'vcs': device_add
<7>PM: Adding info for No Bus:vcs
<7>device: 'vcsa': device_add
<7>PM: Adding info for No Bus:vcsa
<7>device: 'tty1': device_add
<7>PM: Adding info for No Bus:tty1
<7>device: 'tty2': device_add
<7>PM: Adding info for No Bus:tty2
<7>device: 'tty3': device_add
<7>PM: Adding info for No Bus:tty3
<7>device: 'tty4': device_add
<7>PM: Adding info for No Bus:tty4
<7>device: 'tty5': device_add
<7>PM: Adding info for No Bus:tty5
<7>device: 'tty6': device_add
<7>PM: Adding info for No Bus:tty6
<7>device: 'tty7': device_add
<7>PM: Adding info for No Bus:tty7
<7>device: 'tty8': device_add
<7>PM: Adding info for No Bus:tty8
<7>device: 'tty9': device_add
<7>PM: Adding info for No Bus:tty9
<7>device: 'tty10': device_add
<7>PM: Adding info for No Bus:tty10
<7>device: 'tty11': device_add
<7>PM: Adding info for No Bus:tty11
<7>device: 'tty12': device_add
<7>PM: Adding info for No Bus:tty12
<7>device: 'tty13': device_add
<7>PM: Adding info for No Bus:tty13
<7>device: 'tty14': device_add
<7>PM: Adding info for No Bus:tty14
<7>device: 'tty15': device_add
<7>PM: Adding info for No Bus:tty15
<7>device: 'tty16': device_add
<7>PM: Adding info for No Bus:tty16
<7>device: 'tty17': device_add
<7>PM: Adding info for No Bus:tty17
<7>device: 'tty18': device_add
<7>PM: Adding info for No Bus:tty18
<7>device: 'tty19': device_add
<7>PM: Adding info for No Bus:tty19
<7>device: 'tty20': device_add
<7>PM: Adding info for No Bus:tty20
<7>device: 'tty21': device_add
<7>PM: Adding info for No Bus:tty21
<7>device: 'tty22': device_add
<7>PM: Adding info for No Bus:tty22
<7>device: 'tty23': device_add
<7>PM: Adding info for No Bus:tty23
<7>device: 'tty24': device_add
<7>PM: Adding info for No Bus:tty24
<7>device: 'tty25': device_add
<7>PM: Adding info for No Bus:tty25
<7>device: 'tty26': device_add
<7>PM: Adding info for No Bus:tty26
<7>device: 'tty27': device_add
<7>PM: Adding info for No Bus:tty27
<7>device: 'tty28': device_add
<7>PM: Adding info for No Bus:tty28
<7>device: 'tty29': device_add
<7>PM: Adding info for No Bus:tty29
<7>device: 'tty30': device_add
<7>PM: Adding info for No Bus:tty30
<7>device: 'tty31': device_add
<7>PM: Adding info for No Bus:tty31
<7>device: 'tty32': device_add
<7>PM: Adding info for No Bus:tty32
<7>device: 'tty33': device_add
<7>PM: Adding info for No Bus:tty33
<7>device: 'tty34': device_add
<7>PM: Adding info for No Bus:tty34
<7>device: 'tty35': device_add
<7>PM: Adding info for No Bus:tty35
<7>device: 'tty36': device_add
<7>PM: Adding info for No Bus:tty36
<7>device: 'tty37': device_add
<7>PM: Adding info for No Bus:tty37
<7>device: 'tty38': device_add
<7>PM: Adding info for No Bus:tty38
<7>device: 'tty39': device_add
<7>PM: Adding info for No Bus:tty39
<7>device: 'tty40': device_add
<7>PM: Adding info for No Bus:tty40
<7>device: 'tty41': device_add
<7>PM: Adding info for No Bus:tty41
<7>device: 'tty42': device_add
<7>PM: Adding info for No Bus:tty42
<7>device: 'tty43': device_add
<7>PM: Adding info for No Bus:tty43
<7>device: 'tty44': device_add
<7>PM: Adding info for No Bus:tty44
<7>device: 'tty45': device_add
<7>PM: Adding info for No Bus:tty45
<7>device: 'tty46': device_add
<7>PM: Adding info for No Bus:tty46
<7>device: 'tty47': device_add
<7>PM: Adding info for No Bus:tty47
<7>device: 'tty48': device_add
<7>PM: Adding info for No Bus:tty48
<7>device: 'tty49': device_add
<7>PM: Adding info for No Bus:tty49
<7>device: 'tty50': device_add
<7>PM: Adding info for No Bus:tty50
<7>device: 'tty51': device_add
<7>PM: Adding info for No Bus:tty51
<7>device: 'tty52': device_add
<7>PM: Adding info for No Bus:tty52
<7>device: 'tty53': device_add
<7>PM: Adding info for No Bus:tty53
<7>device: 'tty54': device_add
<7>PM: Adding info for No Bus:tty54
<7>device: 'tty55': device_add
<7>PM: Adding info for No Bus:tty55
<7>device: 'tty56': device_add
<7>PM: Adding info for No Bus:tty56
<7>device: 'tty57': device_add
<7>PM: Adding info for No Bus:tty57
<7>device: 'tty58': device_add
<7>PM: Adding info for No Bus:tty58
<7>device: 'tty59': device_add
<7>PM: Adding info for No Bus:tty59
<7>device: 'tty60': device_add
<7>PM: Adding info for No Bus:tty60
<7>device: 'tty61': device_add
<7>PM: Adding info for No Bus:tty61
<7>device: 'tty62': device_add
<7>PM: Adding info for No Bus:tty62
<7>device: 'tty63': device_add
<7>PM: Adding info for No Bus:tty63
<6>Serial: 8250/16550 driver4 ports, IRQ sharing enabled
<7>Registering platform device 'serial8250'. Parent at platform
<7>device: 'serial8250': device_add
<7>bus: 'platform': add device serial8250
<7>PM: Adding info for platform:serial8250
<7>device: 'ttyS0': device_add
<7>PM: Adding info for No Bus:ttyS0
<7>device: 'ttyS1': device_add
<7>PM: Adding info for No Bus:ttyS1
<7>device: 'ttyS2': device_add
<7>PM: Adding info for No Bus:ttyS2
<7>device: 'ttyS3': device_add
<7>PM: Adding info for No Bus:ttyS3
<7>bus: 'platform': add driver serial8250
<7>bus: 'platform': driver_probe_device: matched device serial8250.0 with driver serial8250
<7>bus: 'platform': really_probe: probing driver serial8250 with device serial8250.0
<7>device: 'ttyS0': device_unregister
<7>PM: Removing info for No Bus:ttyS0
<7>device: 'ttyS0': device_create_release
<6>serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
<7>device: 'ttyS0': device_add
<7>PM: Adding info for No Bus:ttyS0
<7>device: 'ttyS1': device_unregister
<7>PM: Removing info for No Bus:ttyS1
<7>device: 'ttyS1': device_create_release
<6>serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
<7>device: 'ttyS1': device_add
<7>PM: Adding info for No Bus:ttyS1
<7>device: 'ttyS2': device_unregister
<7>PM: Removing info for No Bus:ttyS2
<7>device: 'ttyS2': device_create_release
<6>serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
<6>console [ttyS2] enabled
Linux version 2.6.27.18 (srinivas@srinivas-desktop) (gcc version 4.2.1 (CodeSourcery Sourcery G++ Lite 2007q3-51)) #80 Sun Dec 13 17:17:36 IST 2009
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=00c5387f
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
start of evm map io
BUG: mapping for 0x48000000 at 0xd8000000 overlaps vmalloc space
BUG: mapping for 0x48300000 at 0xd8300000 overlaps vmalloc space
BUG: mapping for 0x49000000 at 0xd9000000 overlaps vmalloc space
BUG: mapping for 0x54000000 at 0xe4000000 overlaps vmalloc space
OMAP3430 ES3.1
SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
end of evm map io
CPU0: L1 I VIPT cache. Caches unified at level 2, coherent at level 3
CPU0: Level 1 cache is separate instruction and data
CPU0: I cache: 16384 bytes, associativity 4, 64 byte lines, 64 sets,
supports RA
CPU0: D cache: 16384 bytes, associativity 4, 64 byte lines, 64 sets,
supports RA WB WT
CPU0: Level 2 cache is unified
CPU0: unified cache: 262144 bytes, associativity 8, 64 byte lines, 512 sets,
supports WA RA WB WT
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttyS2,115200n8 noinitrd root=/dev/mmcblk0p2 rw rootfstype=ext3
start of evm irq init
[SRI] start of omap2_clk_init
[SRI] YES, cpu_is_omap34xx
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
[SRI] start of omap3_clkoutx2_recalc
[SRI] end of omap3_clkoutx2_recalc
Clocking rate (Crystal/DPLL/ARM core): 26.0/332/500 MHz
[SRI] start of omap3_clk_lock_dpll5
[SRI] start of omap3_noncore_dpll_set_rate
[SRI] start of _omap3_dpll_compute_freqsel
[SRI] end of _omap3_dpll_compute_freqsel
[SRI] start of omap3_noncore_dpll_program
[SRI] start of _omap3_noncore_dpll_bypass
[SRI] start of _omap3_noncore_dpll_lock
[SRI] start of omap3_dpll_autoidle_read
[SRI] end of omap3_dpll_autoidle_read
[SRI] start of _omap3_dpll_write_clken
[SRI] End of _omap3_dpll_write_clken
[SRI] start of _omap3_wait_dpll_status
[SRI] end of _omap3_wait_dpll_status
[SRI] start of map3_dpll_deny_idle
[SRI] end of map3_dpll_deny_idle
[SRI] end of _omap3_noncore_dpll_lock
[SRI] end of omap3_noncore_dpll_program
[SRI] end of omap3_noncore_dpll_set_rate
[SRI] start of omap3_noncore_dpll_enable
[SRI] start of _omap3_noncore_dpll_lock
[SRI] start of omap3_dpll_autoidle_read
[SRI] end of omap3_dpll_autoidle_read
[SRI] start of _omap3_dpll_write_clken
[SRI] End of _omap3_dpll_write_clken
[SRI] start of _omap3_wait_dpll_status
[SRI] end of _omap3_wait_dpll_status
[SRI] start of map3_dpll_deny_idle
[SRI] end of map3_dpll_deny_idle
[SRI] end of _omap3_noncore_dpll_lock
[SRI] end of omap3_noncore_dpll_enable
[SRI] start of omap3_dpll_allow_idle
[SRI] end of omap3_dpll_allow_idle
[SRI] start of omap3_noncore_dpll_disable
[SRI] start of _omap3_noncore_dpll_stop
[SRI] start of omap3_dpll_autoidle_read
[SRI] end of omap3_dpll_autoidle_read
[SRI] start of _omap3_dpll_write_clken
[SRI] End of _omap3_dpll_write_clken
[SRI] start of omap3_dpll_allow_idle
[SRI] end of omap3_dpll_allow_idle
[SRI] start of _omap3_noncore_dpll_stop
[SRI] start of omap3_noncore_dpll_disable
[SRI] end of omap3_clk_lock_dpll5
[SRI] end of omap2_clk_init
GPMC revision 5.0
IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
Total of 96 interrupts on 1 active controller
OMAP34xx GPIO hardware version 2.5
end of evm irq init
PID hash table entries: 2048 (order: 11, 8192 bytes)
[SRI] start of timer init
OMAP clockevent source: GPTIMER1 at 32768 Hz
hwtimer: Added OMAP2 timer (TI_OMAP2430SDP GP timer 3) at index=0
[SRI] end of timer init
Console: colour dummy device 80x30
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 256MB 256MB = 512MB total
Memory: 514816KB available (3492K code, 513K data, 756K init)
Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
ftrace: allocating 11524 entries in 46 pages
net_namespace: 288 bytes
NET: Registered protocol family 16
[SRI] bus 1 registration start
[SRI] bus 2 registration start
[SRI] bus 2 -- so set the base addr
Serial init start
[SRI] start of omap3_noncore_dpll_enable
[SRI] start of _omap3_noncore_dpll_lock
[SRI] start of omap3_dpll_autoidle_read
[SRI] end of omap3_dpll_autoidle_read
[SRI] start of _omap3_dpll_write_clken
[SRI] End of _omap3_dpll_write_clken
[SRI] start of _omap3_wait_dpll_status
[SRI] end of _omap3_wait_dpll_status
[SRI] start of map3_dpll_deny_idle
[SRI] end of map3_dpll_deny_idle
[SRI] end of _omap3_noncore_dpll_lock
[SRI] end of omap3_noncore_dpll_enable
Serial init end
[SRI] configuring GPIO21 for PHY reset
MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
start of hsmmc init
<7>Registering platform device 'mmci-omap.0'. Parent at platform
end of hsmmc init
<6>start of musb init
end of musb init
[SRI] SETTING THE EHCI MUX...
[SRI] configuring port 1 for PHY mode
MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
[SRI] start of omap2_clk_arch_init
OMAP DMA hardware revision 4.0
USB: No board-specific platform config found
Unable to set the DSSfunctional clock to 432000000
OMAP Display hardware version 2.0
physical address start :0x48070000 end:0x4807003f <6>mapped to :0xd8070000 <6>i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
twl4030: PIH (irq 7) chaining IRQs 368..375
twl4030: power (irq 373) chaining IRQs 376..383
twl4030: gpio (irq 368) chaining IRQs 384..401
physical address start :0x48072000 end:0x4807203f <6>mapped to :0xd8072000 <6>i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
physical address start :0x48060000 end:0x4806003f <6>mapped to :0xd8060000 <6>i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
[SRI] start of twl4030_usb_probe
twl4030_usb twl4030_usb: Initialized TWL4030 USB module
[SRI] end of twl4030_usb_probe
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
musb_hdrc: version 6.0, musb-dma, otg (peripheral+host), debug=0
musb_hdrc: USB OTG mode controller at d80ab000 using DMA, IRQ 92
tracer: 898 pages allocated for 65536 entries of 56 bytes
actual entries 65554
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
NET: Registered protocol family 1
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 1005
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler deadline registered
io scheduler cfq registered
LTT : ltt-relay init
LTT : ltt-ftrace init
[SRI] start of omapfb_init
[SRI] end of omapfb_init
[SRI] In omap3evm_panel_drv_init
[SRI] probing omap3evm_panel_probe
omapfb: configured for panel omap3evm
[SRI] start of omap_dispc_init
<6>omapfb: DISPC version 3.0 initialized
[SRI] end of omap_dispc_init
<6>[SRI] In omap3evm_panel_enable
omapfb: Framebuffer initialized. Total vram 770048 planes 1
omapfb: Pixclock 33230 kHz hfreq 29.9 kHz vfreq 57.2 Hz
[SRI] registered omap3evm_panel
Serial: 8250/16550 driver4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
console [ttyS2] enabled
<7>device: 'ttyS2': device_add
<7>PM: Adding info for No Bus:ttyS2
<7>driver: 'serial8250.0': driver_bound: bound to device 'serial8250'
<7>bus: 'platform': really_probe: bound device serial8250.0 to driver serial8250
<7>bus: 'platform': driver_probe_device: matched device serial8250 with driver serial8250
<7>bus: 'platform': really_probe: probing driver serial8250 with device serial8250
<7>driver: 'serial8250': driver_bound: bound to device 'serial8250'
<7>bus: 'platform': really_probe: bound device serial8250 to driver serial8250
<7>device: 'ram0': device_add
<7>PM: Adding info for No Bus:ram0
<7>device: '1:0': device_add
<7>PM: Adding info for No Bus:1:0
<7>device: 'ram1': device_add
<7>PM: Adding info for No Bus:ram1
<7>device: '1:1': device_add
<7>PM: Adding info for No Bus:1:1
<7>device: 'ram2': device_add
<7>PM: Adding info for No Bus:ram2
<7>device: '1:2': device_add
<7>PM: Adding info for No Bus:1:2
<7>device: 'ram3': device_add
<7>PM: Adding info for No Bus:ram3
<7>device: '1:3': device_add
<7>PM: Adding info for No Bus:1:3
<7>device: 'ram4': device_add
<7>PM: Adding info for No Bus:ram4
<7>device: '1:4': device_add
<7>PM: Adding info for No Bus:1:4
<7>device: 'ram5': device_add
<7>PM: Adding info for No Bus:ram5
<7>device: '1:5': device_add
<7>PM: Adding info for No Bus:1:5
<7>device: 'ram6': device_add
<7>PM: Adding info for No Bus:ram6
<7>device: '1:6': device_add
<7>PM: Adding info for No Bus:1:6
<7>device: 'ram7': device_add
<7>PM: Adding info for No Bus:ram7
<7>device: '1:7': device_add
<7>PM: Adding info for No Bus:1:7
<7>device: 'ram8': device_add
<7>PM: Adding info for No Bus:ram8
<7>device: '1:8': device_add
<7>PM: Adding info for No Bus:1:8
<7>device: 'ram9': device_add
<7>PM: Adding info for No Bus:ram9
<7>device: '1:9': device_add
<7>PM: Adding info for No Bus:1:9
<7>device: 'ram10': device_add
<7>PM: Adding info for No Bus:ram10
<7>device: '1:10': device_add
<7>PM: Adding info for No Bus:1:10
<7>device: 'ram11': device_add
<7>PM: Adding info for No Bus:ram11
<7>device: '1:11': device_add
<7>PM: Adding info for No Bus:1:11
<7>device: 'ram12': device_add
<7>PM: Adding info for No Bus:ram12
<7>device: '1:12': device_add
<7>PM: Adding info for No Bus:1:12
<7>device: 'ram13': device_add
<7>PM: Adding info for No Bus:ram13
<7>device: '1:13': device_add
<7>PM: Adding info for No Bus:1:13
<7>device: 'ram14': device_add
<7>PM: Adding info for No Bus:ram14
<7>device: '1:14': device_add
<7>PM: Adding info for No Bus:1:14
<7>device: 'ram15': device_add
<7>PM: Adding info for No Bus:ram15
<7>device: '1:15': device_add
<7>PM: Adding info for No Bus:1:15
<6>brd: module loaded
brd: module loaded
<7>device: 'loop0': device_add
<7>PM: Adding info for No Bus:loop0
<7>device: '7:0': device_add
<7>PM: Adding info for No Bus:7:0
<7>device: 'loop1': device_add
<7>PM: Adding info for No Bus:loop1
<7>device: '7:1': device_add
<7>PM: Adding info for No Bus:7:1
<7>device: 'loop2': device_add
<7>PM: Adding info for No Bus:loop2
<7>device: '7:2': device_add
<7>PM: Adding info for No Bus:7:2
<7>device: 'loop3': device_add
<7>PM: Adding info for No Bus:loop3
<7>device: '7:3': device_add
<7>PM: Adding info for No Bus:7:3
<7>device: 'loop4': device_add
<7>PM: Adding info for No Bus:loop4
<7>device: '7:4': device_add
<7>PM: Adding info for No Bus:7:4
<7>device: 'loop5': device_add
<7>PM: Adding info for No Bus:loop5
<7>device: '7:5': device_add
<7>PM: Adding info for No Bus:7:5
<7>device: 'loop6': device_add
<7>PM: Adding info for No Bus:loop6
<7>device: '7:6': device_add
<7>PM: Adding info for No Bus:7:6
<7>device: 'loop7': device_add
<7>PM: Adding info for No Bus:loop7
<7>device: '7:7': device_add
<7>PM: Adding info for No Bus:7:7
<6>loop: module loaded
loop: module loaded
<7>bus: 'platform': add driver smc911x
<7>bus: 'platform': driver_probe_device: matched device smc911x with driver smc911x
<7>bus: 'platform': really_probe: probing driver smc911x with device smc911x
<7>device: 'eth0': device_add
<7>PM: Adding info for No Bus:eth0
eth0: LAN9215 (rev 0) at 0x2c000000 IRQ 336eth0: LAN9215 (rev 0) at 0x2c000000 IRQ 336
eth0: Ethernet addr: eth0: Ethernet addr: 50:50:c2:c2:7e:7e:8a:8a:d0:d0:d0
d0
<7>eth0: LAN911x Internal PHY
<7>driver: 'smc911x': driver_bound: bound to device 'smc911x'
<7>bus: 'platform': really_probe: bound device smc911x to driver smc911x
<6>i2c /dev entries driver
i2c /dev entries driver
<7>device class 'i2c-dev': registering
<7>bus: 'i2c': add driver dev_driver
<7>device: 'i2c-1': device_add
<7>PM: Adding info for No Bus:i2c-1
<7>device: 'i2c-2': device_add
<7>PM: Adding info for No Bus:i2c-2
<7>device: 'i2c-3': device_add
<7>PM: Adding info for No Bus:i2c-3
<7>bus: 'i2c': add driver at24
<7>bus: 'i2c': driver_probe_device: matched device 2-00a0 with driver at24
<7>bus: 'i2c': really_probe: probing driver at24 with device 2-00a0
<6>at24 2-00a0: 65536 byte 24c512 EEPROM (writable)
at24 2-00a0: 65536 byte 24c512 EEPROM (writable)
<7>driver: '2-00a0': driver_bound: bound to device 'at24'
<7>bus: 'i2c': really_probe: bound device 2-00a0 to driver at24
<6>start of twl4030_power_init
start of twl4030_power_init
<6>start of config_sleep_wake_sequence
start of config_sleep_wake_sequence
<6>[SRI] P1 LVL wakeup ---config_sleep_wake_sequence
[SRI] P1 LVL wakeup ---config_sleep_wake_sequence
<6>[SRI] P2 LVL wakeup ---config_sleep_wake_sequence
[SRI] P2 LVL wakeup ---config_sleep_wake_sequence
<6>[SRI] P3 LVL wakeup ---config_sleep_wake_sequence
[SRI] P3 LVL wakeup ---config_sleep_wake_sequence
<6>[SRI] End of P1/P2/P3 LVL wakeup ---config_sleep_wake_sequence
[SRI] End of P1/P2/P3 LVL wakeup ---config_sleep_wake_sequence
<6>start of config_warmreset_sequence
start of config_warmreset_sequence
<6>end of config_warmreset_sequence
end of config_warmreset_sequence
<7>device class 'scsi_disk': registering
<4>Driver 'sd' needs updating - please use bus_type methods
Driver 'sd' needs updating - please use bus_type methods
<7>bus: 'scsi': add driver sd
<7>device class 'mtd': registering
<7>bus: 'platform': add driver physmap-flash
<7>device class 'usbmon': registering
<7>device: 'usbmon0': device_add
<7>PM: Adding info for No Bus:usbmon0
<7>ehci_hcd: block sizes: qh 128 qtd 96 itd 160 sitd 96
<7>bus: 'platform': add driver ehci-omap
<7>bus: 'platform': driver_probe_device: matched device ehci-omap.0 with driver ehci-omap
<7>bus: 'platform': really_probe: probing driver ehci-omap with device ehci-omap.0
<7>ehci-omap ehci-omap.0: starting TI EHCI USB Controller
<6>[SRI] start of omap3_noncore_dpll_enable
[SRI] start of omap3_noncore_dpll_enable
<6>[SRI] start of _omap3_noncore_dpll_lock
[SRI] start of _omap3_noncore_dpll_lock
<6>[SRI] start of omap3_dpll_autoidle_read
[SRI] start of omap3_dpll_autoidle_read
<6>[SRI] end of omap3_dpll_autoidle_read
[SRI] end of omap3_dpll_autoidle_read
<6>[SRI] start of _omap3_dpll_write_clken
[SRI] start of _omap3_dpll_write_clken
<6>[SRI] End of _omap3_dpll_write_clken
[SRI] End of _omap3_dpll_write_clken
<6>[SRI] start of omap3_dpll_allow_idle
[SRI] start of omap3_dpll_allow_idle
<6>[SRI] end of omap3_dpll_allow_idle
[SRI] end of omap3_dpll_allow_idle
<6>[SRI] end of _omap3_noncore_dpll_lock
[SRI] end of _omap3_noncore_dpll_lock
<6>[SRI] end of omap3_noncore_dpll_enable
[SRI] end of omap3_noncore_dpll_enable
<7>ehci-omap ehci-omap.0: TLL RESET DONE
<7>ehci-omap ehci-omap.0: OMAP3 ES version > ES2.1
<7>ehci-omap ehci-omap.0: UHH setup done, uhh_hostconfig=21c
<6>ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
<7>device: 'usb_host1': device_add
<7>PM: Adding info for No Bus:usb_host1
<7>drivers/usb/core/inode.c: creating file 'devices'
<7>drivers/usb/core/inode.c: creating file '001'
<7>device: 'usbmon1': device_add
<7>PM: Adding info for No Bus:usbmon1
<6>ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
<7>ehci-omap ehci-omap.0: park 0
<6>ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
<7>ehci-omap ehci-omap.0: reset command 090b02 park=3 ithresh=9 period=1024 Reset HALT
<7>ehci-omap ehci-omap.0: init command 010009 (park)=0 ithresh=1 period=256 RUN
<6>ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00, driver 10 Dec 2004
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00, driver 10 Dec 2004
<7>usb usb1: default language 0x0409
<7>device: 'usb1': device_add
<7>bus: 'usb': add device usb1
<7>PM: Adding info for usb:usb1
<7>usb usb1: uevent
<7>bus: 'usb': driver_probe_device: matched device usb1 with driver usb
<7>bus: 'usb': really_probe: probing driver usb with device usb1
<7>usb usb1: usb_probe_device
<6>usb usb1: configuration #1 chosen from 1 choice
usb usb1: configuration #1 chosen from 1 choice
<7>usb usb1: adding 1-0:1.0 (config #1, interface 0)
<7>device: '1-0:1.0': device_add
<7>bus: 'usb': add device 1-0:1.0
<7>PM: Adding info for usb:1-0:1.0
<7>usb 1-0:1.0: uevent
<7>bus: 'usb': driver_probe_device: matched device 1-0:1.0 with driver hub
<7>bus: 'usb': really_probe: probing driver hub with device 1-0:1.0
<7>hub 1-0:1.0: usb_probe_interface
<7>hub 1-0:1.0: usb_probe_interface - got id
<6>hub 1-0:1.0: USB hub found
hub 1-0:1.0: USB hub found
<6>hub 1-0:1.0: 3 ports detected
hub 1-0:1.0: 3 ports detected
<7>hub 1-0:1.0: standalone hub
<7>hub 1-0:1.0: individual port power switching
<7>hub 1-0:1.0: individual port over-current protection
<7>hub 1-0:1.0: power on to power good time: 20ms
<7>hub 1-0:1.0: local power source is good
<7>hub 1-0:1.0: enabling power on all ports
<7>ehci-omap ehci-omap.0: GetStatus port 2 status 001803 POWER sig=j CSC CONNECT
<7>hub 1-0:1.0: port 2: status 0501 change 0001
<7>driver: '1-0:1.0': driver_bound: bound to device 'hub'
<7>bus: 'usb': really_probe: bound device 1-0:1.0 to driver hub
<7>device class 'usb_endpoint': registering
<7>device: 'usbdev1.1_ep81': device_add
<7>PM: Adding info for No Bus:usbdev1.1_ep81
<7>hub 1-0:1.0: state 7 ports 3 chg 0004 evt 0000
<7>drivers/usb/core/inode.c: creating file '001'
<7>driver: 'usb1': driver_bound: bound to device 'usb'
<7>bus: 'usb': really_probe: bound device usb1 to driver usb
<7>device: 'usbdev1.1_ep00': device_add
<7>PM: Adding info for No Bus:usbdev1.1_ep00
<6>usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
<6>usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>usb usb1: Product: OMAP-EHCI Host Controller
usb usb1: Product: OMAP-EHCI Host Controller
<6>usb usb1: Manufacturer: Linux 2.6.27.18 ehci_hcd
usb usb1: Manufacturer: Linux 2.6.27.18 ehci_hcd
<6>usb usb1: SerialNumber: ehci-omap.0
usb usb1: SerialNumber: ehci-omap.0
<7>driver: 'ehci-omap.0': driver_bound: bound to device 'ehci-omap'
<7>bus: 'platform': really_probe: bound device ehci-omap.0 to driver ehci-omap
<7>hub 1-0:1.0: port 2, status 0501, change 0000, 480 Mb/s
<7>ehci-omap ehci-omap.0: port 2 low speed --> companion
<6>Initializing USB Mass Storage driver...
Initializing USB Mass Storage driver...
<7>bus: 'usb': add driver usb-storage
<7>ehci-omap ehci-omap.0: GetStatus port 2 status 003002 POWER OWNER sig=se0 CSC
<3>hub 1-0:1.0: unable to enumerate USB device on port 2
hub 1-0:1.0: unable to enumerate USB device on port 2
<7>hub 1-0:1.0: state 7 ports 3 chg 0000 evt 0004
<6>usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb-storage
<6>USB Mass Storage support registered.
USB Mass Storage support registered.
<7>bus: 'usb-serial': registered
<7>bus: 'usb': add driver usbserial
<6>usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial
<6>usbserial: USB Serial Driver core
usbserial: USB Serial Driver core
<7>bus: 'usb': add driver usbtest
<6>usbcore: registered new interface driver usbtest
usbcore: registered new interface driver usbtest
<7>bus: 'platform': add driver twl4030_keypad
<7>bus: 'platform': driver_probe_device: matched device twl4030_keypad with driver twl4030_keypad
<7>bus: 'platform': really_probe: probing driver twl4030_keypad with device twl4030_keypad
<7>device: 'input0': device_add
<7>PM: Adding info for No Bus:input0
<6>input: omap_twl4030keypad as /class/input/input0
input: omap_twl4030keypad as /class/input/input0
<7>device: 'event0': device_add
<7>PM: Adding info for No Bus:event0
<7>driver: 'twl4030_keypad': driver_bound: bound to device 'twl4030_keypad'
<7>bus: 'platform': really_probe: bound device twl4030_keypad to driver twl4030_keypad
<7>bus: 'spi': add driver ads7846
<7>bus: 'spi': driver_probe_device: matched device spi1.0 with driver ads7846
<7>bus: 'spi': really_probe: probing driver ads7846 with device spi1.0
<6>ads7846 spi1.0: touchscreen, irq 335
ads7846 spi1.0: touchscreen, irq 335
<7>device: 'input1': device_add
<7>PM: Adding info for No Bus:input1
<6>input: ADS784x Touchscreen as /class/input/input1
input: ADS784x Touchscreen as /class/input/input1
<7>device: 'event1': device_add
<7>PM: Adding info for No Bus:event1
<7>driver: 'spi1.0': driver_bound: bound to device 'ads7846'
<7>bus: 'spi': really_probe: bound device spi1.0 to driver ads7846
<7>bus: 'platform': add driver omap_wdt
<7>bus: 'platform': driver_probe_device: matched device omap_wdt with driver omap_wdt
<7>bus: 'platform': really_probe: probing driver omap_wdt with device omap_wdt
<7>device: 'watchdog': device_add
<7>PM: Adding info for No Bus:watchdog
<6>OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
<7>driver: 'omap_wdt': driver_bound: bound to device 'omap_wdt'
<7>bus: 'platform': really_probe: bound device omap_wdt to driver omap_wdt
<6>cpuidle: using governor ladder
cpuidle: using governor ladder
<6>cpuidle: using governor menu
cpuidle: using governor menu
<7>bus: 'mmc': add driver mmcblk
<7>bus: 'mmc': add driver mmc_test
<6>sdhci: Secure Digital Host Controller Interface driver
sdhci: Secure Digital Host Controller Interface driver
<6>sdhci: Copyright(c) Pierre Ossman
sdhci: Copyright(c) Pierre Ossman
<7>bus: 'platform': add driver mmci-omap
<7>bus: 'platform': driver_probe_device: matched device mmci-omap.0 with driver mmci-omap
<7>bus: 'platform': really_probe: probing driver mmci-omap with device mmci-omap.0
<7>device: 'mmc0': device_add
<7>PM: Adding info for No Bus:mmc0
<7>driver: 'mmci-omap.0': driver_bound: bound to device 'mmci-omap'
<7>bus: 'platform': really_probe: bound device mmci-omap.0 to driver mmci-omap
<7>bus: 'spi': add driver mmc_spi
<7>bus: 'usb': add driver usbhid
<6>usbcore: registered new interface driver usbhid
usbcore: registered new interface driver usbhid
<6>usbhid: v2.6:USB HID core driver
usbhid: v2.6:USB HID core driver
<6>TCP cubic registered
TCP cubic registered
<6>NET: Registered protocol family 17
NET: Registered protocol family 17
<6>NET: Registered protocol family 15
NET: Registered protocol family 15
<6>RPC: Registered udp transport module.
RPC: Registered udp transport module.
<6>RPC: Registered tcp transport module.
RPC: Registered tcp transport module.
<3>Power Management for TI OMAP3.
Power Management for TI OMAP3.
<6>SmartReflex driver initialized
SmartReflex driver initialized
<6>Disabling unused clock "sr2_fck"
Disabling unused clock "sr2_fck"
<6>Disabling unused clock "sr1_fck"
Disabling unused clock "sr1_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt2_ick"
Disabling unused clock "gpt2_ick"
<6>Disabling unused clock "gpt4_ick"
Disabling unused clock "gpt4_ick"
<6>Disabling unused clock "gpt5_ick"
Disabling unused clock "gpt5_ick"
<6>Disabling unused clock "gpt6_ick"
Disabling unused clock "gpt6_ick"
<6>Disabling unused clock "gpt7_ick"
Disabling unused clock "gpt7_ick"
<6>Disabling unused clock "gpt8_ick"
Disabling unused clock "gpt8_ick"
<6>Disabling unused clock "gpt9_ick"
Disabling unused clock "gpt9_ick"
<6>Disabling unused clock "wdt3_ick"
Disabling unused clock "wdt3_ick"
<6>Disabling unused clock "wdt3_fck"
Disabling unused clock "wdt3_fck"
<6>Disabling unused clock "gpio2_dbck"
Disabling unused clock "gpio2_dbck"
<6>Disabling unused clock "gpio3_dbck"
Disabling unused clock "gpio3_dbck"
<6>Disabling unused clock "gpio4_dbck"
Disabling unused clock "gpio4_dbck"
<6>Disabling unused clock "gpio5_dbck"
Disabling unused clock "gpio5_dbck"
<6>Disabling unused clock "gpio6_dbck"
Disabling unused clock "gpio6_dbck"
<6>Disabling unused clock "gpt9_fck"
Disabling unused clock "gpt9_fck"
<6>Disabling unused clock "gpt8_fck"
Disabling unused clock "gpt8_fck"
<6>Disabling unused clock "gpt7_fck"
Disabling unused clock "gpt7_fck"
<6>Disabling unused clock "gpt6_fck"
Disabling unused clock "gpt6_fck"
<6>Disabling unused clock "gpt5_fck"
Disabling unused clock "gpt5_fck"
<6>Disabling unused clock "gpt4_fck"
Disabling unused clock "gpt4_fck"
<6>Disabling unused clock "gpt2_fck"
Disabling unused clock "gpt2_fck"
<6>Disabling unused clock "gpt12_ick"
Disabling unused clock "gpt12_ick"
<6>Disabling unused clock "wdt1_ick"
Disabling unused clock "wdt1_ick"
<6>Disabling unused clock "wdt2_ick"
Disabling unused clock "wdt2_ick"
<6>Disabling unused clock "wdt2_fck"
Disabling unused clock "wdt2_fck"
<6>Disabling unused clock "gpio1_dbck"
Disabling unused clock "gpio1_dbck"
<6>Disabling unused clock "cam_ick"
Disabling unused clock "cam_ick"
<6>Disabling unused clock "cam_mclk"
Disabling unused clock "cam_mclk"
<6>Disabling unused clock "des1_ick"
Disabling unused clock "des1_ick"
<6>Disabling unused clock "sha11_ick"
Disabling unused clock "sha11_ick"
<6>Disabling unused clock "rng_ick"
Disabling unused clock "rng_ick"
<6>Disabling unused clock "aes1_ick"
Disabling unused clock "aes1_ick"
<6>Disabling unused clock "ssi_ick"
Disabling unused clock "ssi_ick"
<6>Disabling unused clock "mailboxes_ick"
Disabling unused clock "mailboxes_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt10_ick"
Disabling unused clock "gpt10_ick"
<6>Disabling unused clock "gpt11_ick"
Disabling unused clock "gpt11_ick"
<6>Disabling unused clock "hdq_ick"
Disabling unused clock "hdq_ick"
<6>Disabling unused clock "mspro_ick"
Disabling unused clock "mspro_ick"
<6>Disabling unused clock "mmchs_ick"
Disabling unused clock "mmchs_ick"
<6>Disabling unused clock "des2_ick"
Disabling unused clock "des2_ick"
<6>Disabling unused clock "sha12_ick"
Disabling unused clock "sha12_ick"
<6>Disabling unused clock "aes2_ick"
Disabling unused clock "aes2_ick"
<6>Disabling unused clock "icr_ick"
Disabling unused clock "icr_ick"
<6>Disabling unused clock "pka_ick"
Disabling unused clock "pka_ick"
<6>Disabling unused clock "ssi_ssr_fck"
Disabling unused clock "ssi_ssr_fck"
<6>Disabling unused clock "hdq_fck"
Disabling unused clock "hdq_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mspro_fck"
Disabling unused clock "mspro_fck"
<6>Disabling unused clock "mmchs_fck"
Disabling unused clock "mmchs_fck"
<6>Disabling unused clock "gpt11_fck"
Disabling unused clock "gpt11_fck"
<6>Disabling unused clock "gpt10_fck"
Disabling unused clock "gpt10_fck"
<6>Disabling unused clock "iva2_ck"
Disabling unused clock "iva2_ck"
<6>Disabling unused clock "dpll4_m6x2_ck"
Disabling unused clock "dpll4_m6x2_ck"
<6>Disabling unused clock "dpll4_m5x2_ck"
Disabling unused clock "dpll4_m5x2_ck"
<6>Disabling unused clock "dpll3_m3x2_ck"
Disabling unused clock "dpll3_m3x2_ck"
<6>Disabling unused clock "sys_clkout1"
Disabling unused clock "sys_clkout1"
<6>VFP support v0.3: VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
implementor 41 architecture 3 part 30 variant c rev 1
<7>device: 'cpu_dma_latency': device_add
<7>PM: Adding info for No Bus:cpu_dma_latency
<7>device: 'network_latency': device_add
<7>PM: Adding info for No Bus:network_latency
<7>device: 'network_throughput': device_add
<7>PM: Adding info for No Bus:network_throughput
<6>Freeing init memory: 756K
Freeing init memory: 756K
mknod: /dev/null: File exists
mknod: /dev/tty: File exists
<4>mmc0: host does not support reading read-only switch. assuming write-enable.
<6>mmc0: new SD card at address b368
<7>device: 'mmc0:b368': device_add
<7>bus: 'mmc': add device mmc0:b368
<7>PM: Adding info for mmc:mmc0:b368
<7>bus: 'mmc': driver_probe_device: matched device mmc0:b368 with driver mmcblk
<7>bus: 'mmc': really_probe: probing driver mmcblk with device mmc0:b368
<6>mmcblk0: mmc0:b368 SDC 2010112KiB
<7>device: 'mmcblk0': device_add
<7>PM: Adding info for No Bus:mmcblk0
<6> mmcblk0: p1 p2
<7>device: 'mmcblk0p1': device_add
<7>PM: Adding info for No Bus:mmcblk0p1
<7>device: 'mmcblk0p2': device_add
<7>PM: Adding info for No Bus:mmcblk0p2
<7>device: '179:0': device_add
<7>PM: Adding info for No Bus:179:0
<7>driver: 'mmc0:b368': driver_bound: bound to device 'mmcblk'
<7>bus: 'mmc': really_probe: bound device mmc0:b368 to driver mmcblk
<6>kjournald starting. Commit interval 5 seconds
<4>EXT3-fs warning: mounting fs with errors, running e2fsck is recommended
<6>EXT3 FS on mmcblk0p2, internal journal
<6>EXT3-fs: recovery complete.
<6>EXT3-fs: mounted filesystem with ordered data mode.
Welcome to InitRAMFS
<7>hub 1-0:1.0: hub_suspend
<7>usb usb1: bus auto-suspend
<7>ehci-omap ehci-omap.0: suspend root hub
init started: BusyBox v1.11.1 (2009-11-20 15:47:58 EST)
/etc/init.d/functions: line 19: /sbin/consoletype: No such file or directory
/etc/init.d/functions: line 61: fstab-decode: command not found
Starting udev: <7>usb usb1: uevent
<7>usb 1-0:1.0: uevent
<7>device: 'eth0': device_rename: renaming to 'eth1'
<6>udev: renamed network interface eth0 to eth1
[ OK ]
/etc/rc.d/init.d/functions: line 19: /sbin/consoletype: No such file or directory
Starting syslog-ng: [ OK ]
Starting lighttpd: /etc/rcS.d/S50lighttpd: line 10: /usr/local/lighttpd/sbin/lighttpd: No such file or directory
/etc/rc.d/init.d/functions: line 19: /sbin/consoletype: No such file or directory
/etc/rcS.d/S55sshd: line 32: runlevel: command not found
Starting sshd: /etc/ssh/sshd_config line 77: Unsupported option GSSAPIAuthentication
/etc/ssh/sshd_config line 79: Unsupported option GSSAPICleanupCredentials
[ OK ]
root@(none):/#
root@(none):/#
------------------------------------------------------------Boot logs end ------------------------------------------------------------------------------------------------------------------------------------