Other Parts Discussed in Thread: TMS320DM368, TPS65510
What the current consumption for the PRTCSS (RTC mode for time tracking) of the DM368?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320DM368, TPS65510
What the current consumption for the PRTCSS (RTC mode for time tracking) of the DM368?
Tom,
Please check the App Note: TMS320DM368 Power Consumption Summary (SPRABB4) which is available from the device Product Folder: http://www.ti.com/product/tms320dm368. There is a spreadsheet which allows you to estimate device power consumption under a number of different use cases. There is support for PRTCSS in this analysis.
Regards.
Tom,
Here are the power numbers you were requesting:
Voltage (V) Power (uW)
=======================
1.2V (core) 91.2
1.8V (IO) 79.2
Power measurements made at 25 degC
Regards.
Hi,
we are using the TPS65510 to power the RTC circuit of the DM368 and we have enabled the RTC. After powering off the board we measure 28,8uA of current drain from the Battery.
Is this correct? is there any way to lower the power consumtion of the RTC of the DM368 ?
Thanks
Sandro