This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

unable to natively build gst-ducati



Hello,

 

I have pandabord running ubuntu 11.10.

I am in process of trying to build gstreamer with neon and other pandaboard optimization flags.

I can build gstreamer (10.35), gst-plugins-base (10.35), and othe pluging successfully.

I cannot build gst-ducati. It is givein lot of errors. Is this project abondoned?

I followed following steps :

      gst clone https://git.gitorious.org/gstreamer-omap/gst-ducati.git

      Then I ran autogen.sh; ./configure. make - but make fails, no such file omap_drm.h, omap_drmif.h, and on and on, then finally missing dmabuff related errors,  dmabuff was supposed to be in gst-plugin-base/gst-lib/gst/. However I did not have it.

    So I cloned  git clone -b dmabuff from above url.

    Then I tried to compile it. It still gives errors,

   What is correct procedure to to build gst-ducati. It is giving lot of grief when I try to build.

   I need to build it, along with all gstreamer plugins that I use, with omap4 optimization flags, such as neon,

   Is there a replacement for gst-ducati?

Thank you

Marc