Hi all,
We have 1.2V,1.8V.3.3V coming up in sequence with a delay of 16msec between each other.
Then the RESET comes up after 250msec.
We can attach with PEEDI Debugger and see registers.
We can't boot from serial even if we have selected BTSEL 2:0 as 011.
We have noticed that PWRCNTON PWRST are floating.
PWRCNTON is unreacheable for us, the second PWRST has been pulled down now with a modification.
So, we'd like "External Reset Mode" but we have this problem.
There is any solution without changing the hardware ?
As the Jtag works can we boot using, at least for a first step, this connection?
Thx