This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

configure minicom to connect to EVM6678 from serial port

Hi

I have connected serial port of EVM6678 to PC (Ubuntu 12.04,  with the included cable) and configure the minicom as follow :

  1. minicom -s
  2. Serial port Setup
  3. Serial Device : /dev/ttyS0
  4. Bps/Par/Bits : 115200 8N1
  5. Enter
  6. exit

and i have set the Switch on the EVM to boot From Linux

but after power on the EVM nothing display on the minicom!

whats the problem? do I need any special Serial Driver?

thans