Hi,
I am trying to add a message for use of ipc in messageq.
The only problem is that for get the right information in the message
I have to consider two dummy variables(reservedX below) to get the right value in my popX
and distanceX variables.
So I don´t know why this behavior.
This is how I define the message:
typedef struct MyMessg{
MessageQ_Msg msg;
int reserved1;
int distance1; int reserved2;int reserved3;
int pop1; int reserved4;int reserved5;
int distance2; int reserved6;int reserved7;
int pop2; int reserved8;int reserved9;
int distance3; int reserved10;int reserved11;
int pop3; int reserved12;int reserved13;
int distance4; int reserved14;int reserved15;
int pop4; int reserved16;int reserved17;
int distance5; int reserved18;int reserved19;
int pop5; int reserved20;int reserved21;
int reserved36;int reserved37;int reserved38;
int distance6; int reserved22;int reserved23;
int pop6; int reserved24;int reserved25;
int distance7; int reserved26;int reserved27;
int pop7; int reserved28;int reserved29;
int offset; int reserved30; int reserved31;
int lenght; int reserved32; int reserved33;
int src_core; int reserved34;int reserved35;
int flag_count;
// myData data;
}MyMsg;
I am using a TMDSEVM6678LE board.
Any help is welcome.
Julian