Other Parts Discussed in Thread: SYSBIOS
Customer is using the following software combination, which appears to be a supported combination based on the release notes of SYSBIOS v6.35.03.47.
CCS v5.40
ControlSuite v3.21
Compiler version TI 6.1.3
SYSBIOS v6.35.3.47
XDCTools v3.25.2.70
Device : TMS320F28069
Under project properties > CCS General > RTSC, we see the System Analyzer (UIA Target) item. We’ve attempted to add this to our project, but have been unable to get it to function properly. Is this even something we should be using?