Hi all,
Iam working on Ti 8107 based DVR , using DVR RDK 3.0. Iam using the 4 channel usecase with HDMI and SD using the different SWMS unit for live display.
I want to get QT graphics + Video in my HDMI and SD display. QT display window is maintained in 1280x720 resolution.
VRAM size 24M and frame buffer allocation to insmod ./kermod/ti81xxfb.ko vram=8M:8M:8M
We start the qt application by the command
./dvrmain -qws hdmi0 hdmi1 -display \"Multi: LinuxFb:/dev/fb0 LinuxFb:/dev/fb2\
In case of SD, the output QT window is cropped. The video is fine in this case, only the graphics get affected.
Is the cropping due to a higher resolution application buffer, used with fb2, which is only 720x480? When I tried with QT window 72x480, The output was fine. So is there a way to increase the fb2 size?
Following a previous thread in e2e, I tried to increase fb2 size using fbset utility , then it was ending up in an error ' out of frame'.
Regards,
Geo