Had anyone tried USB Boot on DM365 (and made it work)?
As far as I understood the chapter on USB boot in sprufg5a, once the BTSEL[2:0] is configured to be "100", the chip will be enumerated by the USB host with some default hardwired settings. I tried it on the EVM with no luck. The host doesn't see it, period.
The doc says: "The RBL must enable the USB pin multiplexing if necessary, since pin multiplexing will not be enabled automatically by the BTSEL[2:0] settings." Is it a statement of a fact, or a suggestion to the developer? Is it possible to change the RBL (ROM Boot Loader) and if yes, how?
Any clarification will be appreciated.