This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6000 gcc toolchain download?

Does anyone know where I can download the C6000 gcc toolchain ( for say Linux or Mac)???

All the links I have found point to CodeSourcery  but go to a general download page with no reference to the C6000 gcc toolchain...

Any ideas???

regards

Anthony

  • Hi Anthony,

    you could use the TI C6000 Compiler which supports gcc. Most of the GCC language extensions are available in the TI compiler when compiling in relaxed ANSI
    mode (--relaxed_ansi) or if the --gcc option is used.

    You can download it from here:

    https://www-a.ti.com/downloads/sds_support/TICodegenerationTools/index.htm

    There's also support in the official GNU Compiler Collection http://gcc.gnu.org/ however I don't think this will provide efficient code (never tried it myself).

    Otherwise I think CodeSourcery is the only option as far as I know.

    Kind regards,

    one and zero

  • Thanks for the reply.

    Can I use the TI C6000 compiler to build the linux as mentioned on http://linux-c6x.org/??

    This site always seems to point one to the CodeSourcery site??

    Do you know how I can actually get the CodeSourcery gcc toolchain.???

    Is it part of the lite version or do you have to pay for it. in the full version...??( I don't mind paying for it etc)

    I have asked a question via there support site but received no reply on how to get access to it...

    I am assuming some sort of relationship between CodeSourcery and Ti in that is was available to downloadin the past . Has all that changed now?

    Regards

    Anthony

  • Please refer to the GCC 4.5.4 link provided in the wiki below:

    http://www.linux-c6x.org/wiki/index.php/Linux-c6x_2.0_Release

    Regards,

    Rahul

    PS: More resources on linux on C6000 is provided here:

    http://processors.wiki.ti.com/index.php/C6000_Linux_Support