I used to work on DM8168, but recently I got a DM8127 camera. Then I tried to run DVR RDK on this camera with the configuration of DM8148. It is strange that the performance is low: enc 1920x1080x23fps + dec 1920x1080x23fps. I think that would be 30fps.
How should I do to improve its performance?
===============================
ARM clk: 600MHz
DDR clk: 400MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF
I2C: ready
DRAM: 512 MiB
NAND: HW ECC BCH8 Selected 256 MiB