This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet RGMII2 in AM335X Adeno BSP

Other Parts Discussed in Thread: AM3358

Relevant Details:
OS: Windows Embedded Compact 7
HW: TI AM3358 processor on custom board
BSP: Windows Embedded Compact 7 TI ARM-A8 BSP Version 02.30.00 From Adeneo Embedded

Hi,

so the AM3358 processor has 2 Ethernet ports on it, RGMII2 Ethernet interface would be the second of these ports I assume.  In the Adeneo Embedded Windows Embedded Compact 7 TI ARM-A8 BSP Version 02.30.00 would it still be the AM_DEVICE_CPGMAC0 device and clocks that are used for RGMII2? Or is there such a thing as CPGMAC1 on the AM3358 which represents port 2?

Thanks

John