This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Yocto Filesystem



Hi,


I am trying to build "OMAP5 GLSDK". 6.01 version

I ran in to build issues

ERROR: Task 2595 (/home/abhijitlocal/ti-glsdk_omap5-uevm_6_01_00_01/oe-layersetup/sources/oe-core/meta/recipes-graphics/directfb/directfb_1.6.1.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3825 tasks of which 2957 didn't need to be rerun and 1 failed.
No currently running tasks (3825 of 3877)

looks like open gl lilbrary is not downloaded and installed as part of the recipe.Any help how do i fix this.

For now i manually disabled the build "MESA" from DirectFB-1.6.1/system/Makefile.

Build goes through but but again fails in the last stage

ERROR: Function failed: do_rootfs (see /home/abhijitlocal/ti-glsdk_omap5-uevm_6_01_00_01/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/omap5_evm-oe-linux-gnueabi/tisdk-rootfs-image-1.0-r0/temp/log.do_rootfs.6428 for further information)
ERROR: Task 8 (/home/abhijitlocal/ti-glsdk_omap5-uevm_6_01_00_01/oe-layersetup/sources/meta-arago/meta-arago-distro/recipes-core/images/tisdk-rootfs-image.bb, do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3876 tasks of which 2972 didn't need to be rerun and 1 failed.
No currently running tasks (3876 of 3877)

Summary: 1 task failed:
/home/abhijitlocal/ti-glsdk_omap5-uevm_6_01_00_01/oe-layersetup/sources/meta-arago/meta-arago-distro/recipes-core/images/tisdk-rootfs-image.bb, do_rootfs
S

Am i missing something..

Thanks

Vijay