Hi Experts,
I am encountering the above mentioned error if I try to recompile my project for Cortex-A8 with the GNU compiler tools. Error comes up during linking phase. I do not see any compiler errors when compiling with the TI compiler tools. It seems that the TSK_idle definition is not present when using the GNU compiler tools or am I missing something?
Used tools:
xdc_3_25_00_48
bios_6_35_01_29
CCSv5.4.xxx77 with gcc-arm-none-eabi-4_7-2012q4
Any hints to solve this issue would be greatly appreciated.
Many thanks and best regards,
GINNI