What steps are necessary to configure IPV6 for a dhcp client? Or how do I manually config an IPv6 address. I'm not using XGCONF, just calling CfgAddEntry.
I looked through the CfgAddEntry code and there does not seem to be a way to add an entry for an IPv6 interface. I assume this has to be done to get the ipv6 interface added in.
What I'm ultimately trying to do is bind to an ipv6 socket (IP_ANYADDR --- all 0's) and receive a broadcast packet. I get through the socket creation and binding process without error, but when I call recvfrom on the socket, it never returns. I have two threads, one is ipv4 and the other ipv6. My test program is sending two broadcast packets, ipv4 and ipv6, and I see both of them in wireshark, but I only receive the ipv4 packet.
Thanks
Milan