This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help reduce power on C6748 - peripherals question



Customer asks:

If a peripheral will never be used and I want to minimize power consumption, what should be done with it's power pins?  For example I am using USB0 but not USB1.  I am not using the SATA controller.  Leave SATA_VDD and SATA-VSS unconnected.  What for the VDDs for USB1?

It is possible to run the bank containing EMIF on the 6748 at 1.8V.  I will take advantage of this feature.  Unfortunately the JTAG is also in this power group "B" with the EMIF.  The Emulators seem to run on 3.3V.  Is there a preferred method for level translation across this interface?  I notice the EMU[1:0] pins are bi-directional.