This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with SGX-driver loading on Beaglebone Black

Hi all,

I'm trying to install SGX-driver for Bealgebone Black. But the driver cannot be loaded.

Modprobe  pvrsrvkm doesn't get warning or error. However, the module still not be loaded when checking with lsmod.

I'm using SGX-SDK from 

http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/gfxsdk/latest//exports/Graphics_SDK_setuplinux_4_10_00_01_hardfp_minimal_demos.bin

With build option:

make BUILD=release OMAPES=8.x FBDEV=yes SUPPORT_XORG=0 all_km
sudo make BUILD=release OMAPES=8.x SUPPORT_XORG=0 EGLIMAGE=1 install_km

The toolchain is linaro-toolchain-4.7

My current kernel is Rowboat kernel 3.2.0 with linaro-nano rootfs (a minimal ubuntu-based rootfs). After running modprobe pvrsrvkm, I see that there's information from dmesg:

[    0.000000] Linux version 3.2.0 (hieppham@PC1705) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 Fri Aug 2 16:12:34 ICT 2013
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] On node 0 totalpages: 131072
[    0.000000] free_area_init_node: node 0, pgdat c066bd54, node_mem_map c06a5000
[    0.000000]   Normal zone: 1024 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 130048 pages, LIFO batch:31
[    0.000000] AM335X ES2.0 (sgx neon )
[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[    0.000000] pcpu-alloc: [0] 0 
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=UUID=55c46ee3-f603-4268-a8d7-31b79c519271 rootwait ro
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 512MB = 512MB total
[    0.000000] Memory: 510504k/510504k available, 13784k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc05d8000   (5952 kB)
[    0.000000]       .init : 0xc05d8000 - 0xc0612000   ( 232 kB)
[    0.000000]       .data : 0xc0612000 - 0xc0674b50   ( 395 kB)
[    0.000000]        .bss : 0xc0674b74 - 0xc06a4ea0   ( 193 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000152] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
[    0.048736] pid_max: default: 32768 minimum: 301
[    0.048889] Security Framework initialized
[    0.048980] Mount-cache hash table entries: 512
[    0.049438] CPU: Testing write buffer coherency: ok
[    0.050292] devtmpfs: initialized
[    0.071197] omap_hwmod: pruss: failed to hardreset
[    0.072479] print_constraints: dummy: 
[    0.072937] NET: Registered protocol family 16
[    0.075500] OMAP GPIO hardware version 0.1
[    0.078826] omap_mux_init: Add partition: #1: core, flags: 0
[    0.081237]  omap_i2c.1: alias fck already exists
[    0.082305]  omap2_mcspi.1: alias fck already exists
[    0.082580]  omap2_mcspi.2: alias fck already exists
[    0.082916]  edma.0: alias fck already exists
[    0.082946]  edma.0: alias fck already exists
[    0.082977]  edma.0: alias fck already exists
[    0.115447] bio: create slab <bio-0> at 0
[    0.118164] SCSI subsystem initialized
[    0.120208] usbcore: registered new interface driver usbfs
[    0.120605] usbcore: registered new interface driver hub
[    0.120849] usbcore: registered new device driver usb
[    0.121032] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[    0.121368] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[    0.122741] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.124450] tps65910 1-002d: could not be detected
[    0.126098] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.127593] Switching to clocksource gp timer
[    0.150482] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.150665] musb-hdrc musb-hdrc.0: dma type: pio
[    0.151062] MUSB0 controller's USBSS revision = 4ea20800
[    0.151092] musb0: Enabled SW babble control
[    0.151092] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[    0.151123] musb-hdrc: MHDRC RTL version 2.0 
[    0.151153] musb-hdrc: setup fifo_mode 4
[    0.151184] musb-hdrc: 28/31 max ep, 16384/16384 memory
[    0.151184] musb-hdrc.0: bulk split disabled
[    0.151214] musb-hdrc.0: bulk combine disabled
[    0.151885] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using PIO, IRQ 18
[    0.152099] musb-hdrc musb-hdrc.1: dma type: pio
[    0.152465] MUSB1 controller's USBSS revision = 4ea20800
[    0.152496] musb1: Enabled SW babble control
[    0.152526] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[    0.152526] musb-hdrc: MHDRC RTL version 2.0 
[    0.152557] musb-hdrc: setup fifo_mode 4
[    0.152587] musb-hdrc: 28/31 max ep, 16384/16384 memory
[    0.152587] musb-hdrc.1: bulk split disabled
[    0.152618] musb-hdrc.1: bulk combine disabled
[    0.152709] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.152801] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.152954] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.152954] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.152984] usb usb1: Product: MUSB HDRC host driver
[    0.152984] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[    0.153015] usb usb1: SerialNumber: musb-hdrc.1
[    0.154144] hub 1-0:1.0: USB hub found
[    0.154205] hub 1-0:1.0: 1 port detected
[    0.154968] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using PIO, IRQ 19
[    0.155456] NET: Registered protocol family 2
[    0.155700] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.156066] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    0.156463] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[    0.156677] TCP: Hash tables configured (established 16384 bind 16384)
[    0.156677] TCP reno registered
[    0.156707] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.156738] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.156982] NET: Registered protocol family 1
[    0.157318] RPC: Registered named UNIX socket transport module.
[    0.157318] RPC: Registered udp transport module.
[    0.157348] RPC: Registered tcp transport module.
[    0.157348] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.157592] Trying to unpack rootfs image as initramfs...
[    0.418243] Freeing initrd memory: 2440K
[    0.418273] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.439270] VFS: Disk quotas dquot_6.5.2
[    0.439331] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.440246] msgmni has been set to 1001
[    0.441192] io scheduler noop registered
[    0.441223] io scheduler deadline registered
[    0.441284] io scheduler cfq registered (default)
[    0.442779] Could not set LED4 to fully on
[    0.459472] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    1.033386] console [ttyO0] enabled
[    1.037750] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    1.045715] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    1.053680] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    1.061614] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    1.069641] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    1.077972] [drm] Initialized drm 1.1.0 20060810
[    1.095336] brd: module loaded
[    1.105377] loop: module loaded
[    1.109222] i2c-core: driver [tsl2550] using legacy suspend method
[    1.115692] i2c-core: driver [tsl2550] using legacy resume method
[    1.122192] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.188110] usb 1-1: new low-speed USB device number 2 using musb-hdrc
[    1.194976] No daughter card found on AM335x EVM
[    1.199890] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.215118] Board name: A335BNLT
[    1.218505] Board version: 0A5A
[    1.221832] The board is a AM335x Beaglebone Black.
[    1.229156] tps65217 1-0024: TPS65217 ID 0xe version 1.2
[    1.236999] print_constraints: DCDC1: 900 <--> 1800 mV at 1500 mV 
[    1.245758] print_constraints: DCDC2: 900 <--> 3300 mV at 1100 mV 
[    1.254455] print_constraints: DCDC3: 900 <--> 1500 mV at 1100 mV 
[    1.263153] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV 
[    1.271911] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV 
[    1.280517] print_constraints: LDO3: 1800 <--> 3300 mV at 1800 mV 
[    1.289184] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV 
[    1.297088]  omap_hsmmc.0: alias fck already exists
[    1.302642]  omap_hsmmc.1: alias fck already exists
[    1.308166]  omap_i2c.3: alias fck already exists
[    1.313507] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[    1.320800]  davinci-mcasp.0: alias fck already exists
[    1.328552] at24 3-0054: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.335845] IN : bone_setup_display_daughter_board 
[    1.371795] usb 1-1: New USB device found, idVendor=413c, idProduct=2105
[    1.378814] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    1.386291] usb 1-1: Product: Dell USB Keyboard
[    1.391021] usb 1-1: Manufacturer: Dell
[    1.408172] No display cape found on BeagleBone
[    1.413543]  da8xx_lcdc.0: alias fck already exists
[    1.419189] da8xx_lcdc da8xx_lcdc.0: GLCD: Found nxp-1280x720@60 panel
[    1.447784] Console: switching to colour frame buffer device 160x45
[    1.600799] tda998x 1-0070: found TDA19988
[    1.732635] tda998x 1-0070: Connected to an HDMI monitor with cea mode 2
[    1.769775] Setup HDMI display complete
[    1.774047] at24 3-0055: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.781341] IN : bone_setup_daughter_board 
[    1.858276] at24 3-0056: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.865539] IN : bone_setup_daughter_board 
[    1.928253] at24 3-0057: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.935516] IN : bone_setup_daughter_board 
[    2.000732] mtdoops: mtd device (mtddev=name/number) must be supplied
[    2.007965] omap2-nand driver initializing
[    2.012512] OneNAND driver initializing
[    2.018310] CAN device driver interface
[    2.022338] CAN bus driver for Bosch D_CAN controller 1.0
[    2.078399] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    2.084869] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    2.093750] davinci_mdio.0: probed
[    2.097351] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[    2.106414] usbcore: registered new interface driver zd1201
[    2.112518] usbcore: registered new interface driver cdc_ether
[    2.118835] usbcore: registered new interface driver cdc_eem
[    2.124969] usbcore: registered new interface driver dm9601
[    2.130828] cdc_ncm: 04-Aug-2011
[    2.134429] usbcore: registered new interface driver cdc_ncm
[    2.140350] Initializing USB Mass Storage driver...
[    2.145751] usbcore: registered new interface driver usb-storage
[    2.152069] USB Mass Storage support registered.
[    2.157623] mousedev: PS/2 mouse device common for all mice
[    2.164916] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[    2.172241] i2c /dev entries driver
[    2.176788] Linux video capture interface: v2.00
[    2.182098] usbcore: registered new interface driver uvcvideo
[    2.188110] USB Video Class driver (1.1.1)
[    2.195800] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    2.278656] cpuidle: using governor ladder
[    2.283569] cpuidle: using governor menu
[    2.303558] input: Dell Dell USB Keyboard as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1:1.0/input/input0
[    2.315948] generic-usb 0003:413C:2105.0001: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-musb-hdrc.1-1/input0
[    2.328369] usbcore: registered new interface driver usbhid
[    2.334289] usbhid: USB HID core driver
[    2.342773] usbcore: registered new interface driver snd-usb-audio
[    2.351654] ALSA device list:
[    2.354797]   No soundcards found.
[    2.358398] oprofile: hardware counters not available
[    2.363739] oprofile: using timer interrupt.
[    2.368255] nf_conntrack version 0.5.0 (8014 buckets, 32056 max)
[    2.375213] ip_tables: (C) 2000-2006 Netfilter Core Team
[    2.381011] TCP cubic registered
[    2.384399] NET: Registered protocol family 17
[    2.389099] can: controller area network core (rev 20090105 abi 8)
[    2.395721] NET: Registered protocol family 29
[    2.400421] can: raw protocol (rev 20090105)
[    2.404907] can: broadcast manager protocol (rev 20090105 t)
[    2.410949] Registering the dns_resolver key type
[    2.415954] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    2.424072] ThumbEE CPU extension supported.
[    2.428649] mux: Failed to setup hwmod io irq -22
[    2.434356] Power Management for AM33XX family
[    2.439270] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    2.446014] Copied the M3 firmware to UMEM
[    2.450408] Cortex M3 Firmware Version = 0x181
[    2.458953] clock: disabling unused clocks to save power
[    2.470275] Detected MACID=c8:a0:30:ae:80:98
[    2.476074] cpsw: Detected MACID = c8:a0:30:ae:80:9a
[    2.482635] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[    2.492370] Freeing init memory: 232K
[    2.533905] mmc0: host does not support reading read-only switch. assuming write-enable.
[    2.547576] mmc0: new high speed SDHC card at address aaaa
[    2.565460] mmcblk0: mmc0:aaaa SU04G 3.69 GiB 
[    2.579071]  mmcblk0: p1 p2
[    2.620544] udevd[649]: starting version 175
[    3.028900] mmc1: new high speed MMC card at address 0001
[    3.063171] mmcblk1: mmc1:0001 MMC02G 1.78 GiB 
[    3.103088] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB
[    3.119934] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB
[    3.175292]  mmcblk1: p1 p2
[    3.243621]  mmcblk1boot1: unknown partition table
[    3.282989]  mmcblk1boot0: unknown partition table
[    3.327362] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[    3.335144] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[    3.739807] EXT4-fs (mmcblk0p2): recovery complete
[    3.757598] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    4.307952] init: ureadahead main process (740) terminated with status 5
[    4.887298] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[    5.533660] udevd[807]: starting version 175
[    8.388214] init: plymouth main process (741) killed by ABRT signal
[    8.396820] init: plymouth-splash main process (945) terminated with status 2
[    9.819274] init: plymouth-stop pre-start process (1030) terminated with status 1
[   10.385803] init: tty1 main process (1032) killed by TERM signal
[  131.006774] init: plymouth-stop pre-start process (1152) terminated with status 1
[  243.499114] Disabling lock debugging due to kernel taint
[  243.540191] ------------[ cut here ]------------
[  243.540252] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x88/0xa8()
[  243.540283] sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
[  243.540313] Modules linked in: pvrsrvkm(O+)
[  243.540344] Backtrace: 
[  243.540405] [<c00181b4>] (dump_backtrace+0x0/0x10c) from [<c0449f44>] (dump_stack+0x18/0x1c)
[  243.540435]  r6:c00fbbd8 r5:00000009 r4:df545d38 r3:c0636c0c
[  243.540527] [<c0449f2c>] (dump_stack+0x0/0x1c) from [<c003efec>] (warn_slowpath_common+0x54/0x6c)
[  243.540588] [<c003ef98>] (warn_slowpath_common+0x0/0x6c) from [<c003f0a8>] (warn_slowpath_fmt+0x38/0x40)
[  243.540618]  r8:00000001 r7:df282000 r6:df282000 r5:df2b9a40 r4:ffffffef
[  243.540649] r3:00000009
[  243.540679] [<c003f070>] (warn_slowpath_fmt+0x0/0x40) from [<c00fbbd8>] (sysfs_add_one+0x88/0xa8)
[  243.540710]  r3:df282000 r2:c054f578
[  243.540771] [<c00fbb50>] (sysfs_add_one+0x0/0xa8) from [<c00fc474>] (sysfs_do_create_link+0xf8/0x1e0)
[  243.540802]  r7:df545d90 r6:df013db0 r5:df2b9a40 r4:df2b9b30
[  243.540863] [<c00fc37c>] (sysfs_do_create_link+0x0/0x1e0) from [<c00fc570>] (sysfs_create_link+0x14/0x18)
[  243.540924] [<c00fc55c>] (sysfs_create_link+0x0/0x18) from [<c02573ac>] (bus_add_device+0xcc/0x184)
[  243.540985] [<c02572e0>] (bus_add_device+0x0/0x184) from [<c0255714>] (device_add+0x458/0x594)
[  243.541015]  r8:00000000 r7:c064f150 r6:bf01eee8 r5:00000000 r4:bf01eee0
[  243.541046] r3:00000000
[  243.541107] [<c02552bc>] (device_add+0x0/0x594) from [<c0259a1c>] (platform_device_add+0xfc/0x1e8)
[  243.541137] [<c0259920>] (platform_device_add+0x0/0x1e8) from [<c0259d54>] (platform_device_register+0x28/0x2c)
[  243.541168]  r7:df544000 r6:c0674b80 r5:bf020d94 r4:bf01eed8
[  243.541473] [<c0259d2c>] (platform_device_register+0x0/0x2c) from [<bf02b078>] (PVRCore_Init+0x78/0x168 [pvrsrvkm])
[  243.541503]  r4:00000000 r3:00000000
[  243.541656] [<bf02b000>] (PVRCore_Init+0x0/0x168 [pvrsrvkm]) from [<c000876c>] (do_one_initcall+0x128/0x1a8)
[  243.541687]  r6:c0674b80 r5:bf01f11c r4:bf01f11c
[  243.541748] [<c0008644>] (do_one_initcall+0x0/0x1a8) from [<c006b3e8>] (sys_init_module+0x3e4/0x1b68)
[  243.541809] [<c006b004>] (sys_init_module+0x0/0x1b68) from [<c0014740>] (ret_fast_syscall+0x0/0x30)
[  243.541839] ---[ end trace d042962694bc9021 ]---
 

I'm not sure why the module cannot be loaded, it was compiled with the kernel, so I think it can't be mismatch.

I followed the instruction from http://processors.wiki.ti.com/index.php/SGXDbg#Unable_to_install_the_kernel_modules_.28pvrsrvkm.ko_or_omaplfb.ko.29

But it seems not to work. My output of gfx_check.sh is as follow:

WSEGL settings
[default]
WindowSystem=libpvrPVR2D_FRONTWSEGL.so
#WindowSystem=libpvrPVR2D_FLIPWSEGL.so

------
ARM CPU information
Processor	: ARMv7 Processor rev 2 (v7l)
BogoMIPS	: 598.76
Features	: swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls 
CPU implementer	: 0x41
CPU architecture: 7
CPU variant	: 0x3
CPU part	: 0xc08
CPU revision	: 2

Hardware	: am335xevm
Revision	: 0000
Serial		: 0000000000000000
------
SGX driver information
cat: /proc/pvr/version: No such file or directory
------
Framebuffer settings

mode "1280x720-75"
    # D: 92.756 MHz, H: 56.318 kHz, V: 75.191 Hz
    geometry 1280 720 1280 1440 16
    timings 10781 219 109 19 5 39 5
    rgba 5/11,6/5,5/0,0/0
endmode

Frame buffer device information:
    Name        : DA8xx FB Drv
    Address     : 0x9e000000
    Size        : 3686400
    Type        : PACKED PIXELS
    Visual      : TRUECOLOR
    XPanStep    : 0
    YPanStep    : 1
    YWrapStep   : 0
    LineLength  : 2560
    Accelerator : No
------
Rotation settings
0
------
Kernel Module information
Module                  Size  Used by
------
Boot settings
console=ttyO0,115200n8 root=UUID=55c46ee3-f603-4268-a8d7-31b79c519271 rootwait ro
------
Linux Kernel version
Linux localhost.localdomain 3.2.0 #1 Fri Aug 2 16:12:34 ICT 2013 armv7l armv7l armv7l GNU/Linux

I don't know where I am wrong, any help will be greatly appreciate.

Thanks a lot,

Hiep.