This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Clock Transition Mode Settings

The CLKTRCTRL Bits in the CLKSTCTRL registers are used to select the Clock Transition Mode.

While a NO_SLEEP is set, Sleep transition cannot be initiated.
Does it mean that a Clock Domain never changes in the ACTIVE state?

While a SW_SLEEP is set, the software-forced sleep transition is initiated when the associated hardware conditions are satisfied.
Do the conditions mean the conditions of the IDLE_TRANSITION state?

Once a SW_WKUP is set, is the wake-up transition initiated unconditionally?

Best regards,

Daisuke