Hi,
The EtherCAT Slave have the description in the following file:
EtherCAT_IPCore_Xilinx_V2_04a_Datasheet_all_v1i0.pdf
Does it mean always need to access full Sync Manager buffer when cyclic Process Data.
In TI case:
SM 2 (Outputs) is defined 5 Bytes which consisted sDOOutputs(1 Byte) & sDO1Outputs(4 Bytes).
And in the cyclic frame, the Logic address is 0x1000000 and the data is five Bytes.
Questions:
1. When I send a frame which the Logic address is 0x1000000 and the data is 1 Byte for sDOOutputs.LEDs, does it will be success?(Can write to the memory of SM2, and will generation the "HOST_AL_EVENT" ?)
2. When I send a frame which the Logic address is 0x1000003 and the data is 2 Byte for sDO1Outputs.Motordata, does it will be success?
3. If I want send the sDOOutputs and the sDO1Outputs in different cyclic time, have any suggestion?(Assign two Sync Manager for Process Output Data?)
Best regards,
Louis chou