Are there any routing examples using the AM335x and 2 8-bit DDR3/L SDRAMs in 6 layers? I have seen the Beagle Bone Black which uses 6-layers and DDR3 but it is 1 16-bit SDRAM. I would like to be able to use the full 1 GB addressability of the AM335X.