Hi,
When using the sound driver for the dm365 on the montevista kernel I find that it takes about 1% of the CPU bandwidth at 8KHz but rises to 99% of the CPU bandwidth when running at 11025 Hz.
I am using the CQ93VC codec which only seems to work with ALSA.
I need to run at least at 11025 Hz as this is the minimum sample rate that works with the ittium aaclc encoder. I would prefer to work at a higher sample rate.
Are there any other sample rates that work well with the Montevista sound driver?
Will things be any better with the TI kernel sound driver?
regards,
Shlomo