Hi,
I want to boot TI813x_EVM board using sd card but it is giving following error :
U-Boot 2010.06 (Nov 26 2012 - 11:30:03)
TI813X-GP rev 1.0
ARM clk: 720MHz
DDR clk: 533MHz
L3 clk: 200MHz
IVA clk: 410MHz
ISS clk: 480MHz
DSS clk: 200MHz
DSP clk: 750MHz
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0
Using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till TI813X_EVM prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0
mmc_send_cmd: timedout waiting for cmddis!
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
## Starting application at 0x80800000 ...
ÿï÷}ægcso#@@
Can anyone please help me to solve this ?