Hi,
I am working on DM3730 Mistral EVM.
I am trying to run the video loopback application from composite input(CVBS) to LCD output.
I am using DVSDK_4306 - Linux 2.6.37
For this, I am running the following application from the filesystem:
/usr/share/ti/ti-dmai-apps/video_loopback_copy_dm3730.x470MV -O lcd -I composite
When I run this application, I see the following error messages:
Capture: Current Input: camera
VIDIOC_S_INPUT: Invalid argument
Capture: Input changed to: camera
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
.
.
.
Please find the complete boot message below:
OMAP3_EVM # print
bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
bootdelay=10
baudrate=115200
bootfile=uImage
loadaddr=0x82000000
usbtty=cdc_acm
console=ttyO0,115200n8
mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omap_vout.vid1_static_vrfb_alloc=y
nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2
loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
loaduimage=fatload mmc 0 ${loadaddr} uImage
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
nandboot=echo Booting from nand ...; run nandargs; onenand read ${loadaddr} 280000 400000; bootm ${loadaddr}
stdin=serial
stdout=serial
stderr=serial
dieid#=219800011ff0000001592f350100301d
ethact=smc911x-0
Environment size: 909/131068 bytes
OMAP3_EVM # boot
mmc1 is available
reading boot.scr
302 bytes read
Running bootscript from mmc ...
## Executing script at 82000000
reading uImage
3289936 bytes read
## Booting kernel from Legacy Image at 80200000 ...
Image Name: Arago/2.6.37-psp04.02.00.07.sdk/
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3289872 Bytes = 3.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 2.6.37 (a0876316@bangdvsdkdev01) (gcc version 4.3.3 (GCC) ) #1 Thu Dec 22 23:02:19 IST 2011
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP3 EVM
[ 0.000000] Reserving 4194304 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP3630 ES1.1 (l2cache iva sgx neon isp 192mhz_clk )
[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 45312
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw ip=off mem=55M@0x80000000 mpurate=1000 omap_vout.vid1_static_vrfb_alloc=y omapfb.vram=0:4M mem=128M@0x88000000 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 55MB 124MB = 179MB total
[ 0.000000] Memory: 167756k/167756k available, 19636k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc003f000 ( 220 kB)
[ 0.000000] .text : 0xc003f000 - 0xc06254ec (6042 kB)
[ 0.000000] .data : 0xc0626000 - 0xc07e8560 (1802 kB)
[ 0.000000] NR_IRQS:409
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/1000 MHz
[ 0.000000] omap_hwmod: i2c1: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c2: softreset failed (waited 10000 usec)
[ 0.000000] omap_hwmod: i2c3: softreset failed (waited 10000 usec)
[ 0.000000] Reprogramming SDRC clock to 400000000 Hz
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] GPMC revision 5.0
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install interrupt handler for IRQ407
[ 0.000000] Trying to install interrupt handler for IRQ408
[ 0.000000] Trying to install type control for IRQ409
[ 0.000000] Trying to set irq flags for IRQ409
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.000000] ... MAX_LOCK_DEPTH: 48
[ 0.000000] ... MAX_LOCKDEP_KEYS: 8191
[ 0.000000] ... CLASSHASH_SIZE: 4096
[ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384
[ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768
[ 0.000000] ... CHAINHASH_SIZE: 16384
[ 0.000000] memory used by lock dependency info: 3951 kB
[ 0.000000] per task-struct memory footprint: 2304 bytes
[ 0.000000] Calibrating delay loop... 998.84 BogoMIPS (lpj=3899392)
[ 0.000000] pid_max: default: 32768 minimum: 301
[ 0.000000] Security Framework initialized
[ 0.000000] Mount-cache hash table entries: 512
[ 0.000000] CPU: Testing write buffer coherency: ok
[ 0.000000] regulator: core version 0.5
[ 0.000000] regulator: dummy:
[ 0.000000] NET: Registered protocol family 16
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/clock.c:438 omap2_clk_switch_mpurate_at_boot+0x80/0xb4()
[ 0.000000] clock: dpll1_ck: unable to set MPU rate to 1000: -22
[ 0.000000] Modules linked in:
[ 0.000000] [<c004faf0>] (unwind_backtrace+0x0/0xec) from [<c00790c4>] (warn_slowpath_common+0x4c/0x64)
[ 0.000000] [<c00790c4>] (warn_slowpath_common+0x4c/0x64) from [<c0079170>] (warn_slowpath_fmt+0x30/0x40)
[ 0.000000] [<c0079170>] (warn_slowpath_fmt+0x30/0x40) from [<c00138ac>] (omap2_clk_switch_mpurate_at_boot+0x80/0xb4)
[ 0.000000] [<c00138ac>] (omap2_clk_switch_mpurate_at_boot+0x80/0xb4) from [<c00138ec>] (omap3xxx_clk_arch_init+0xc/0x3c)
[ 0.000000] [<c00138ec>] (omap3xxx_clk_arch_init+0xc/0x3c) from [<c003f3c8>] (do_one_initcall+0xc8/0x198)
[ 0.000000] [<c003f3c8>] (do_one_initcall+0xc8/0x198) from [<c000869c>] (kernel_init+0x98/0x150)
[ 0.000000] [<c000869c>] (kernel_init+0x98/0x150) from [<c004ad10>] (kernel_thread_exit+0x0/0x8)
[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---
[ 0.000000] OMAP DMA hardware revision 5.0
[ 0.078796] bio: create slab <bio-0> at 0
[ 0.082275] regulator: vwl1271: 1800 mV
[ 0.085998] SCSI subsystem initialized
[ 0.094757] usbcore: registered new interface driver usbfs
[ 0.095672] usbcore: registered new interface driver hub
[ 0.096313] usbcore: registered new device driver usb
[ 0.112854] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
[ 0.120666] twl4030: PIH (irq 7) chaining IRQs 368..375
[ 0.120788] twl4030: power (irq 373) chaining IRQs 376..383
[ 0.122436] twl4030: gpio (irq 368) chaining IRQs 384..401
[ 0.134429] regulator: VIO: 1800 mV normal standby
[ 0.136352] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
[ 0.138305] regulator: VDAC: 1800 mV normal standby
[ 0.140106] regulator: VAUX2_4030: 2800 mV normal standby
[ 0.141998] regulator: VPLL2: 1800 mV normal standby
[ 0.143859] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
[ 0.145782] regulator: VAUX3: 2800 mV normal standby
[ 0.146636] omap_device: omap_i2c.1: new worst case deactivate latency 0: 30517
[ 0.146881] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.159637] omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
[ 0.163879] Advanced Linux Sound Architecture Driver Version 1.0.23.
[ 0.166442] Bluetooth: Core ver 2.15
[ 0.167022] NET: Registered protocol family 31
[ 0.167022] Bluetooth: HCI device and connection manager initialized
[ 0.167114] Bluetooth: HCI socket layer initialized
[ 0.168823] Switching to clocksource 32k_counter
[ 0.252807] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
[ 0.253082] musb-hdrc musb-hdrc.0: dma type: dma-inventra
[ 0.253784] musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
[ 0.255218] NET: Registered protocol family 2
[ 0.255615] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.256774] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.257019] TCP bind hash table entries: 8192 (order: 6, 360448 bytes)
[ 0.259552] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.259613] TCP reno registered
[ 0.259643] UDP hash table entries: 128 (order: 1, 12288 bytes)
[ 0.259826] UDP-Lite hash table entries: 128 (order: 1, 12288 bytes)
[ 0.260467] NET: Registered protocol family 1
[ 0.261505] RPC: Registered udp transport module.
[ 0.261505] RPC: Registered tcp transport module.
[ 0.261535] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.262207] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.264984] omap_device: omap_i2c.1: new worst case activate latency 0: 61035
[ 0.267150] omap3evm camera init done successfully...
[ 0.267669] omap-iommu omap-iommu.0: isp registered
[ 0.268249] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3EVM)
[ 0.371826] VFS: Disk quotas dquot_6.5.2
[ 0.371917] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.373718] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.374359] msgmni has been set to 327
[ 0.378326] io scheduler noop registered
[ 0.378326] io scheduler deadline registered
[ 0.378479] io scheduler cfq registered (default)
[ 0.442626] OMAP DSS rev 2.0
[ 0.442962] OMAP DISPC rev 3.0
[ 0.443054] OMAP VENC rev 2
[ 0.443817] OMAP DSI rev 1.0
[ 0.773437] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.779266] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 1.612915] console [ttyO0] enabled
[ 1.617858] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 1.626251] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 1.634643] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
[ 1.671539] brd: module loaded
[ 1.688842] loop: module loaded
[ 1.698242] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.705108] omap2-nand driver initializing
[ 1.709960] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix )
[ 1.716888] Creating 5 MTD partitions on "omap2-nand.0":
[ 1.722442] 0x000000000000-0x000000080000 : "X-Loader-NAND"
[ 1.734588] 0x000000080000-0x0000001c0000 : "U-Boot-NAND"
[ 1.745056] 0x0000001c0000-0x000000280000 : "Boot Env-NAND"
[ 1.755615] 0x000000280000-0x000000780000 : "Kernel-NAND"
[ 1.767639] 0x000000780000-0x000020000000 : "File System - NAND"
[ 2.017730] OneNAND driver initializing
[ 2.022064] omap2-onenand omap2-onenand: Cannot request GPMC CS
[ 2.028442] omap2-onenand: probe of omap2-onenand failed with error -16
[ 2.038269] smsc911x: Driver version 2008-10-21.
[ 2.048095] smsc911x-mdio: probed
[ 2.052032] eth0: attached PHY driver [SMSC LAN8700] (mii_bus:phy_addr=ffffffff:01, irq=-1)
[ 2.062225] net eth0: MAC Address: 00:50:c2:7e:96:63
[ 2.068572] usbcore: registered new interface driver asix
[ 2.074676] usbcore: registered new interface driver cdc_ether
[ 2.081298] usbcore: registered new interface driver net1080
[ 2.087738] usbcore: registered new interface driver cdc_subset
[ 2.094390] usbcore: registered new interface driver zaurus
[ 2.100311] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.114257] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 3.121398] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 3.129699] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 3.145599] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 3.152191] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.159332] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.166931] usb usb1: Product: OMAP-EHCI Host Controller
[ 3.172515] usb usb1: Manufacturer: Linux 2.6.37 ehci_hcd
[ 3.178161] usb usb1: SerialNumber: ehci-omap.0
[ 3.186523] hub 1-0:1.0: USB hub found
[ 3.190551] hub 1-0:1.0: 3 ports detected
[ 3.224365] Initializing USB Mass Storage driver...
[ 3.230072] usbcore: registered new interface driver usb-storage
[ 3.236389] USB Mass Storage support registered.
[ 3.241821] usbcore: registered new interface driver usbtest
[ 3.247863] g_ether gadget: using random self ethernet address
[ 3.253997] g_ether gadget: using random host ethernet address
[ 3.261596] usb0: MAC de:fc:ed:60:01:fc
[ 3.265686] usb0: HOST MAC 06:0b:2c:0a:49:1b
[ 3.270172] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
[ 3.277160] g_ether gadget: g_ether ready
[ 3.281372] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 3.287139] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 3.295867] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.303039] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.310607] usb usb2: Product: MUSB HDRC host driver
[ 3.315795] usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
[ 3.321472] usb usb2: SerialNumber: musb-hdrc.0
[ 3.328765] hub 2-0:1.0: USB hub found
[ 3.332794] hub 2-0:1.0: 1 port detected
[ 3.340759] mice: PS/2 mouse device common for all mice
[ 3.348968] input: TWL4030 Keypad as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/twl4030_keypad/input/input0
[ 3.366729] ads7846 spi1.0: touchscreen, irq 335
[ 3.373535] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input1
[ 3.387817] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input2
[ 3.402069] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 3.408935] twl_rtc twl_rtc: Power up reset detected.
[ 3.415008] twl_rtc twl_rtc: Enabling TWL-RTC.
[ 3.421325] i2c /dev entries driver
[ 3.429565] Linux media interface: v0.10
[ 3.434143] Linux video capture interface: v2.00
[ 3.441070] omap3isp supply VDD_CSIPHY1 not found, using dummy regulator
[ 3.448181] omap3isp supply VDD_CSIPHY2 not found, using dummy regulator
[ 3.455596] omap3isp omap3isp: Revision 15.0 found
[ 3.460876] omap-iommu omap-iommu.0: isp: version 1.1
[ 3.533935] mt9t111 2-003c: Unable to detectmt9t111sensor
[ 3.544708] isp_register_subdev_group: Unable to register subdev mt9t111
[ 3.553100] tvp514x 3-005c: tvp514x 3-005c decoder driver registered !!
[ 3.564056] tvp514x 3-005c: tvp5146m2 (Version - 0x03) found at 0xb8 (OMAP I2C adapter)
[ 3.579376] usbcore: registered new interface driver uvcvideo
[ 3.585449] USB Video Class driver (v1.0.0)
[ 3.590087] omap_device: omap_wdt.-1: new worst case activate latency 0: 30517
[ 3.599151] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 3.605468] omap_device: omap_wdt.-1: new worst case deactivate latency 0: 30517
[ 3.613800] Bluetooth: HCI UART driver ver 2.2
[ 3.618499] Bluetooth: HCI H4 protocol initialized
[ 3.623535] Bluetooth: HCILL protocol initialized
[ 3.636505] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator
[ 3.649383] usbcore: registered new interface driver usbhid
[ 3.655273] usbhid: USB HID core driver
[ 3.661834] usbcore: registered new interface driver snd-usb-audio
[ 3.671966] OMAP3 EVM SoC init
[ 3.676849] omap_device: omap_i2c.1: new worst case deactivate latency 0: 61035
[ 3.772003] asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok
[ 3.783691] ALSA device list:
[ 3.786895] #0: omap3evm
[ 3.789703] oprofile: hardware counters not available
[ 3.795013] oprofile: using timer interrupt.
[ 3.799621] nf_conntrack version 0.5.0 (2621 buckets, 10484 max)
[ 3.807250] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.813354] TCP cubic registered
[ 3.816741] Initializing XFRM netlink socket
[ 3.821380] NET: Registered protocol family 17
[ 3.826141] NET: Registered protocol family 15
[ 3.831390] Bluetooth: L2CAP ver 2.15
[ 3.835266] Bluetooth: L2CAP socket layer initialized
[ 3.840606] Bluetooth: SCO (Voice Link) ver 0.6
[ 3.845367] Bluetooth: SCO socket layer initialized
[ 3.850891] Bluetooth: RFCOMM TTY layer initialized
[ 3.856018] Bluetooth: RFCOMM socket layer initialized
[ 3.861450] Bluetooth: RFCOMM ver 1.11
[ 3.865386] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.870941] Bluetooth: BNEP filters: protocol multicast
[ 3.876434] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.884094] Registering the dns_resolver key type
[ 3.889495] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 3.901672] ThumbEE CPU extension supported.
[ 3.917602] Power Management for TI OMAP3.
[ 3.922515] sr_init: No PMIC hook to init smartreflex
[ 3.928253] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 3.936889] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 3.949066] SmartReflex Class3 initialized
[ 3.983917] clock: disabling unused clocks to save power
[ 3.991394] platform mpu.0: omap_voltage_scale: Already at the requestedrate 1000000000
[ 4.094055] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 4.102844] omap_vout omap_vout: Buffer Size = 3686400
[ 4.121337] omap_vout omap_vout: : registered and initialized video device 16
[ 4.128906] omap_vout omap_vout: Buffer Size = 3686400
[ 4.136077] omap_vout omap_vout: : registered and initialized video device 17
[ 4.147491] Waiting for root device /dev/mmcblk0p2...
[ 4.169097] mmc0: new high speed SDHC card at address b368
[ 4.176818] mmcblk0: mmc0:b368 USD 3.75 GiB
[ 4.186645] mmcblk0: p1 p2
[ 4.269927] EXT3-fs: barriers not enabled
[ 10.545654] kjournald starting. Commit interval 5 seconds
[ 10.917144] EXT3-fs (mmcblk0p2): using internal journal
[ 10.922698] EXT3-fs (mmcblk0p2): recovery complete
[ 10.931701] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 10.939361] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 10.945800] Freeing init memory: 220K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
[ 11.718750] udevd (735): /proc/735/oom_adj is deprecated, please use /proc/735/oom_score_adj instead.
Remounting root file system...
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
ALSA: Restoring mixer settings...
No state is present for card omap3evm
Found hardware: "" "" "" "" ""
Hardware is initialized using a generic method
Configuring network interfaces... No state is present for card omap3evm
[ 27.751403] net eth0: SMSC911x/921x identified at 0xd0884000, IRQ: 336
eth0 no wireless extensions.
udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
Fri Dec 23 00:34:00 UTC 2011
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
[ 41.609100]
[ 41.609130] =============================================
[ 41.616302] [ INFO: possible recursive locking detected ]
[ 41.621948] 2.6.37 #1
[ 41.624328] ---------------------------------------------
[ 41.629943] pvrsrvinit/2142 is trying to acquire lock:
[ 41.635314] (psPVRSRVMutex){+.+.+.}, at: [<bf00bbc8>] PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm]
[ 41.644561]
[ 41.644561] but task is already holding lock:
[ 41.650634] (psPVRSRVMutex){+.+.+.}, at: [<bf00eb34>] PVRSRV_BridgeDispatchKM+0x20/0x16c [pvrsrvkm]
[ 41.660247]
[ 41.660247] other info that might help us debug this:
[ 41.667083] 1 lock held by pvrsrvinit/2142:
[ 41.671447] #0: (psPVRSRVMutex){+.+.+.}, at: [<bf00eb34>] PVRSRV_BridgeDispatchKM+0x20/0x16c [pvrsrvkm]
[ 41.681518]
[ 41.681518] stack backtrace:
[ 41.686096] [<c004faf0>] (unwind_backtrace+0x0/0xec) from [<c00a91ac>] (__lock_acquire+0xf98/0x18d0)
[ 41.695648] [<c00a91ac>] (__lock_acquire+0xf98/0x18d0) from [<c00a9bb8>] (lock_acquire+0xd4/0xf4)
[ 41.704925] [<c00a9bb8>] (lock_acquire+0xd4/0xf4) from [<c047375c>] (mutex_lock_nested+0x5c/0x2d8)
[ 41.714324] [<c047375c>] (mutex_lock_nested+0x5c/0x2d8) from [<bf00bbc8>] (PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm])
[ 41.725433] [<bf00bbc8>] (PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm]) from [<bf00e944>] (OSAllocPages_Impl+0x68/0xa4 [pvrsrvkm])
[ 41.737426] [<bf00e944>] (OSAllocPages_Impl+0x68/0xa4 [pvrsrvkm]) from [<bf0052e8>] (BM_ImportMemory+0xe4/0x290 [pvrsrvkm])
[ 41.749145] [<bf0052e8>] (BM_ImportMemory+0xe4/0x290 [pvrsrvkm]) from [<bf009b0c>] (RA_Alloc+0xb4/0x288 [pvrsrvkm])
[ 41.760131] [<bf009b0c>] (RA_Alloc+0xb4/0x288 [pvrsrvkm]) from [<bf004cb0>] (BM_Alloc+0xa8/0x280 [pvrsrvkm])
[ 41.770477] [<bf004cb0>] (BM_Alloc+0xa8/0x280 [pvrsrvkm]) from [<bf00aac0>] (AllocDeviceMem+0x80/0x108 [pvrsrvkm])
[ 41.781402] [<bf00aac0>] (AllocDeviceMem+0x80/0x108 [pvrsrvkm]) from [<bf00afd8>] (_PVRSRVAllocDeviceMemKM+0x80/0x158 [pvrsrvkm])
[ 41.793670] [<bf00afd8>] (_PVRSRVAllocDeviceMemKM+0x80/0x158 [pvrsrvkm]) from [<bf015190>] (PVRSRVAllocDeviceMemBW+0x9c/0x1a0 [pvrsrvkm])
[ 41.806701] [<bf015190>] (PVRSRVAllocDeviceMemBW+0x9c/0x1a0 [pvrsrvkm]) from [<bf012d24>] (BridgedDispatchKM+0xd4/0x12c [pvrsrvkm])
[ 41.819152] [<bf012d24>] (BridgedDispatchKM+0xd4/0x12c [pvrsrvkm]) from [<bf00ec28>] (PVRSRV_BridgeDispatchKM+0x114/0x16c [pvrsrvkm])
[ 41.831756] [<bf00ec28>] (PVRSRV_BridgeDispatchKM+0x114/0x16c [pvrsrvkm]) from [<c0116cf8>] (do_vfs_ioctl+0x4e0/0x54c)
[ 41.842956] [<c0116cf8>] (do_vfs_ioctl+0x4e0/0x54c) from [<c0116db4>] (sys_ioctl+0x50/0x74)
[ 41.851684] [<c0116db4>] (sys_ioctl+0x50/0x74) from [<c0049cc0>] (ret_fast_syscall+0x0/0x3c)
[ 41.901855] CMEMK module: built on Dec 22 2011 at 23:52:43
[ 41.907684] Reference Linux version 2.6.37
[ 41.912139] File /datalocal/DVSDK43_HPDL380G7/arago-tmp/work/dm37x-evm-arago-linux-gnueabi/ti-linuxutils-1_2_26_02_05-r102d/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
[ 41.930938] CMEM Range Overlaps Kernel Physical - allowing overlap
[ 41.937438] CMEM phys_start (0x83700000) overlaps kernel (0x80000000 -> 0x8b300000)
[ 41.946868] allocated heap buffer 0xd2000000 of size 0x2200000
[ 41.953002] heap fallback enabled - will try heap if pool buffer is not available
[ 41.960876] cmemk initialized
[ 42.061828] DSPLINK Module (1.65.01.05_eng) created on Date: Dec 22 2011 Time: 23:55:34
[ 42.868041] SDMAK module: built on Dec 22 2011 at 23:52:50
[ 42.873870] Reference Linux version 2.6.37
[ 42.878326] File /datalocal/DVSDK43_HPDL380G7/arago-tmp/work/dm37x-evm-arago-linux-gnueabi/ti-linuxutils-1_2_26_02_05-r102d/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/sdma/src/module/sdmak.c
numid=49,iface=MIXER,name='HeadsetL Mixer AudioL1'
; type=BOOLEAN,access=rw------,values=1
: values=on
numid=46,iface=MIXER,name='HeadsetR Mixer AudioR1'
; type=BOOLEAN,access=rw------,values=1
: values=on
Simple mixer control 'Headset',0
Capabilities: pvolume penum
Playback channels: Front Left - Front Right
Limits: Playback 0 - 3
Mono:
Front Left: Playback 1 [33%] [-6.00dB]
Front Right: Playback 1 [33%] [-6.00dB]
Starting Matrix GUI application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dm37x-evm ttyO0
Arago 2011.06 dm37x-evm ttyO0
dm37x-evm login: root
root@dm37x-evm:~# /usr/share/ti/ti-dmai-apps/video_loopback_copy_dm3730.x470MV -
O lcd -I composite
Media: Opened Media Device
Enumerating media entities
[1]:OMAP3 ISP CCP2
[2]:OMAP3 ISP CCP2 input
[3]:OMAP3 ISP CSI2a
[4]:OMAP3 ISP CSI2a output
[5]:OMAP3 ISP CCDC
[6]:OMAP3 ISP CCDC output
[7]:OMAP3 ISP preview
[8]:OMAP3 ISP preview input
[9]:OMAP3 ISP preview output
[10]:OMAP3 ISP resizer
[11]:OMAP3 ISP resizer input
[12]:OMAP3 ISP resizer output
[13]:OMAP3 ISP AEWB
[14]:OMAP3 ISP AF
[15]:OMAP3 ISP histogram
[17]:tvp514x 3-005c
[17]:tvp514x 3-005c
Total number of entities: 17
Enumerating links/pads for entities
pads for entity 1=(0 INPUT) (1 OUTPUT)
[1:1]===>[5:0] INACTIVE
pads for entity 2=(0 OUTPUT)
[2:0]===>[1:0] INACTIVE
pads for entity 3=(0 INPUT) (1 OUTPU[ 72.254028] tvp514x 3-005c: tvp5146m2 (Version - 0x03) found at 0xb8 (OMAP I2C adapter)
T)
[3:1]===>[4:0] INACTIVE
[3:1]===>[5:0] INACTIVE
pads for entity 4=(0 INPUT)
pads for entity 5=(0 INPUT) (1 OUTPUT) (2 OUTPUT)
[5:1]===>[6:0] INACTIVE
[5:2]===>[7:0] INACTIVE
[5:1]===>[10:0] INACTIVE
[5:2]===>[13:0] ACTIVE
[5:2]===>[14:0] ACTIVE
[5:2]===>[15:0] ACTIVE
pads for entity 6=(0 INPUT)
pads for entity 7=(0 INPUT) (1 OUTPUT)
[7:1]===>[9:0] INACTIVE
[7:1]===>[10:0] INACTIVE
pads for entity 8=(0 OUTPUT)
[8:0]===>[7:0] INACTIVE
pads for entity 9=(0 INPUT)
pads for entity 10=(0 INPUT) (1 OUTPUT)
[10:1]===>[12:0] INACTIVE
pads for entity 11=(0 OUTPUT)
[11:0]===>[10:0] INACTIVE
pads for entity 12=(0 INPUT)
pads for entity 13=(0 INPUT)
pads for entity 14=(0 INPUT)
pads for entity 15=(0 INPUT)
pads for entity 17=(0 OUTPUT)
[17:0]===>[5:0] INACTIVE
pads for entity 17=(0 OUTPUT)
[17:0]===>[5:0] INACTIVE
Enabling link [tvp5146]===>[ccdc]
[tvp514x]===>[ccdc] enabled
Enabling link [ccdc]===>[video_node]
[ccdc]===>[video_node] enabled
Capture: Current Input: camera
VIDIOC_S_INPUT: Invalid argument
Capture: Input changed to: camera
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Invalid argument
VIDIOC_ENUMSTD: Inval
root@dm37x-evm:~#
The same application with DVSDK_4206(Linux 2.6.32) is working fine.
Please let me know if you need more info on the same.
Regards,
Bharath S
OMAP3_EVM # print bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi bootdelay=10 baudrate=115200 bootfile=uImage loadaddr=0x82000000 usbtty=cdc_acm console=ttyO0,115200n8 mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait omap_vout.vid1_static_vrfb_alloc=y nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2 loadbootscript=fatload mmc 0 ${loadaddr} boot.scr bootscript=echo Running bootscript from mmc ...; source ${loadaddr} loaduimage=fatload mmc 0 ${loadaddr} uImage mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr} nandboot=echo Booting from nand ...; run nandargs; onenand read ${loadaddr} 280000 400000; bootm ${loadaddr} stdin=serial stdout=serial stderr=serial dieid#=219800011ff0000001592f350100301d ethact=smc911x-0 Environment size: 909/131068 bytes OMAP3_EVM # boot mmc1 is available reading boot.scr 302 bytes read Running bootscript from mmc ... ## Executing script at 82000000 reading uImage 3289936 bytes read ## Booting kernel from Legacy Image at 80200000 ... Image Name: Arago/2.6.37-psp04.02.00.07.sdk/ Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3289872 Bytes = 3.1 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 2.6.37 (a0876316@bangdvsdkdev01) (gcc version 4.3.3 (GCC) ) #1 Thu Dec 22 23:02:19 IST 2011 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f [ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: OMAP3 EVM [ 0.000000] Reserving 4194304 bytes SDRAM for VRAM [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] OMAP3630 ES1.1 (l2cache iva sgx neon isp 192mhz_clk ) [ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 45312 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw ip=off mem=55M@0x80000000 mpurate=1000 omap_vout.vid1_static_vrfb_alloc=y omapfb.vram=0:4M mem=128M@0x88000000 rootwait [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 55MB 124MB = 179MB total [ 0.000000] Memory: 167756k/167756k available, 19636k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB) [ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .init : 0xc0008000 - 0xc003f000 ( 220 kB) [ 0.000000] .text : 0xc003f000 - 0xc06254ec (6042 kB) [ 0.000000] .data : 0xc0626000 - 0xc07e8560 (1802 kB) [ 0.000000] NR_IRQS:409 [ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/1000 MHz [ 0.000000] omap_hwmod: i2c1: softreset failed (waited 10000 usec) [ 0.000000] omap_hwmod: i2c2: softreset failed (waited 10000 usec) [ 0.000000] omap_hwmod: i2c3: softreset failed (waited 10000 usec) [ 0.000000] Reprogramming SDRC clock to 400000000 Hz [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts [ 0.000000] Total of 96 interrupts on 1 active controller [ 0.000000] GPMC revision 5.0 [ 0.000000] Trying to install interrupt handler for IRQ402 [ 0.000000] Trying to install interrupt handler for IRQ403 [ 0.000000] Trying to install interrupt handler for IRQ404 [ 0.000000] Trying to install interrupt handler for IRQ405 [ 0.000000] Trying to install interrupt handler for IRQ406 [ 0.000000] Trying to install interrupt handler for IRQ407 [ 0.000000] Trying to install interrupt handler for IRQ408 [ 0.000000] Trying to install type control for IRQ409 [ 0.000000] Trying to set irq flags for IRQ409 [ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz [ 0.000000] Console: colour dummy device 80x30 [ 0.000000] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar [ 0.000000] ... MAX_LOCKDEP_SUBCLASSES: 8 [ 0.000000] ... MAX_LOCK_DEPTH: 48 [ 0.000000] ... MAX_LOCKDEP_KEYS: 8191 [ 0.000000] ... CLASSHASH_SIZE: 4096 [ 0.000000] ... MAX_LOCKDEP_ENTRIES: 16384 [ 0.000000] ... MAX_LOCKDEP_CHAINS: 32768 [ 0.000000] ... CHAINHASH_SIZE: 16384 [ 0.000000] memory used by lock dependency info: 3951 kB [ 0.000000] per task-struct memory footprint: 2304 bytes [ 0.000000] Calibrating delay loop... 998.84 BogoMIPS (lpj=3899392) [ 0.000000] pid_max: default: 32768 minimum: 301 [ 0.000000] Security Framework initialized [ 0.000000] Mount-cache hash table entries: 512 [ 0.000000] CPU: Testing write buffer coherency: ok [ 0.000000] regulator: core version 0.5 [ 0.000000] regulator: dummy: [ 0.000000] NET: Registered protocol family 16 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] OMAP GPIO hardware version 2.5 [ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.000000] ------------[ cut here ]------------ [ 0.000000] WARNING: at arch/arm/mach-omap2/clock.c:438 omap2_clk_switch_mpurate_at_boot+0x80/0xb4() [ 0.000000] clock: dpll1_ck: unable to set MPU rate to 1000: -22 [ 0.000000] Modules linked in: [ 0.000000] [<c004faf0>] (unwind_backtrace+0x0/0xec) from [<c00790c4>] (warn_slowpath_common+0x4c/0x64) [ 0.000000] [<c00790c4>] (warn_slowpath_common+0x4c/0x64) from [<c0079170>] (warn_slowpath_fmt+0x30/0x40) [ 0.000000] [<c0079170>] (warn_slowpath_fmt+0x30/0x40) from [<c00138ac>] (omap2_clk_switch_mpurate_at_boot+0x80/0xb4) [ 0.000000] [<c00138ac>] (omap2_clk_switch_mpurate_at_boot+0x80/0xb4) from [<c00138ec>] (omap3xxx_clk_arch_init+0xc/0x3c) [ 0.000000] [<c00138ec>] (omap3xxx_clk_arch_init+0xc/0x3c) from [<c003f3c8>] (do_one_initcall+0xc8/0x198) [ 0.000000] [<c003f3c8>] (do_one_initcall+0xc8/0x198) from [<c000869c>] (kernel_init+0x98/0x150) [ 0.000000] [<c000869c>] (kernel_init+0x98/0x150) from [<c004ad10>] (kernel_thread_exit+0x0/0x8) [ 0.000000] ---[ end trace 1b75b31a2719ed1c ]--- [ 0.000000] OMAP DMA hardware revision 5.0 [ 0.078796] bio: create slab <bio-0> at 0 [ 0.082275] regulator: vwl1271: 1800 mV [ 0.085998] SCSI subsystem initialized [ 0.094757] usbcore: registered new interface driver usbfs [ 0.095672] usbcore: registered new interface driver hub [ 0.096313] usbcore: registered new device driver usb [ 0.112854] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz [ 0.120666] twl4030: PIH (irq 7) chaining IRQs 368..375 [ 0.120788] twl4030: power (irq 373) chaining IRQs 376..383 [ 0.122436] twl4030: gpio (irq 368) chaining IRQs 384..401 [ 0.134429] regulator: VIO: 1800 mV normal standby [ 0.136352] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby [ 0.138305] regulator: VDAC: 1800 mV normal standby [ 0.140106] regulator: VAUX2_4030: 2800 mV normal standby [ 0.141998] regulator: VPLL2: 1800 mV normal standby [ 0.143859] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby [ 0.145782] regulator: VAUX3: 2800 mV normal standby [ 0.146636] omap_device: omap_i2c.1: new worst case deactivate latency 0: 30517 [ 0.146881] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz [ 0.159637] omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz [ 0.163879] Advanced Linux Sound Architecture Driver Version 1.0.23. [ 0.166442] Bluetooth: Core ver 2.15 [ 0.167022] NET: Registered protocol family 31 [ 0.167022] Bluetooth: HCI device and connection manager initialized [ 0.167114] Bluetooth: HCI socket layer initialized [ 0.168823] Switching to clocksource 32k_counter [ 0.252807] musb-hdrc: version 6.0, otg (peripheral+host), debug=0 [ 0.253082] musb-hdrc musb-hdrc.0: dma type: dma-inventra [ 0.253784] musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92 [ 0.255218] NET: Registered protocol family 2 [ 0.255615] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.256774] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.257019] TCP bind hash table entries: 8192 (order: 6, 360448 bytes) [ 0.259552] TCP: Hash tables configured (established 8192 bind 8192) [ 0.259613] TCP reno registered [ 0.259643] UDP hash table entries: 128 (order: 1, 12288 bytes) [ 0.259826] UDP-Lite hash table entries: 128 (order: 1, 12288 bytes) [ 0.260467] NET: Registered protocol family 1 [ 0.261505] RPC: Registered udp transport module. [ 0.261505] RPC: Registered tcp transport module. [ 0.261535] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.262207] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.264984] omap_device: omap_i2c.1: new worst case activate latency 0: 61035 [ 0.267150] omap3evm camera init done successfully... [ 0.267669] omap-iommu omap-iommu.0: isp registered [ 0.268249] AM37x/DM37x Linux PSP version 04.02.00.07 (OMAP3EVM) [ 0.371826] VFS: Disk quotas dquot_6.5.2 [ 0.371917] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.373718] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.374359] msgmni has been set to 327 [ 0.378326] io scheduler noop registered [ 0.378326] io scheduler deadline registered [ 0.378479] io scheduler cfq registered (default) [ 0.442626] OMAP DSS rev 2.0 [ 0.442962] OMAP DISPC rev 3.0 [ 0.443054] OMAP VENC rev 2 [ 0.443817] OMAP DSI rev 1.0 [ 0.773437] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.779266] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0 [ 1.612915] console [ttyO0] enabled [ 1.617858] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1 [ 1.626251] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2 [ 1.634643] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3 [ 1.671539] brd: module loaded [ 1.688842] loop: module loaded [ 1.698242] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.705108] omap2-nand driver initializing [ 1.709960] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix ) [ 1.716888] Creating 5 MTD partitions on "omap2-nand.0": [ 1.722442] 0x000000000000-0x000000080000 : "X-Loader-NAND" [ 1.734588] 0x000000080000-0x0000001c0000 : "U-Boot-NAND" [ 1.745056] 0x0000001c0000-0x000000280000 : "Boot Env-NAND" [ 1.755615] 0x000000280000-0x000000780000 : "Kernel-NAND" [ 1.767639] 0x000000780000-0x000020000000 : "File System - NAND" [ 2.017730] OneNAND driver initializing [ 2.022064] omap2-onenand omap2-onenand: Cannot request GPMC CS [ 2.028442] omap2-onenand: probe of omap2-onenand failed with error -16 [ 2.038269] smsc911x: Driver version 2008-10-21. [ 2.048095] smsc911x-mdio: probed [ 2.052032] eth0: attached PHY driver [SMSC LAN8700] (mii_bus:phy_addr=ffffffff:01, irq=-1) [ 2.062225] net eth0: MAC Address: 00:50:c2:7e:96:63 [ 2.068572] usbcore: registered new interface driver asix [ 2.074676] usbcore: registered new interface driver cdc_ether [ 2.081298] usbcore: registered new interface driver net1080 [ 2.087738] usbcore: registered new interface driver cdc_subset [ 2.094390] usbcore: registered new interface driver zaurus [ 2.100311] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 3.114257] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller [ 3.121398] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1 [ 3.129699] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800 [ 3.145599] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00 [ 3.152191] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 3.159332] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 3.166931] usb usb1: Product: OMAP-EHCI Host Controller [ 3.172515] usb usb1: Manufacturer: Linux 2.6.37 ehci_hcd [ 3.178161] usb usb1: SerialNumber: ehci-omap.0 [ 3.186523] hub 1-0:1.0: USB hub found [ 3.190551] hub 1-0:1.0: 3 ports detected [ 3.224365] Initializing USB Mass Storage driver... [ 3.230072] usbcore: registered new interface driver usb-storage [ 3.236389] USB Mass Storage support registered. [ 3.241821] usbcore: registered new interface driver usbtest [ 3.247863] g_ether gadget: using random self ethernet address [ 3.253997] g_ether gadget: using random host ethernet address [ 3.261596] usb0: MAC de:fc:ed:60:01:fc [ 3.265686] usb0: HOST MAC 06:0b:2c:0a:49:1b [ 3.270172] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008 [ 3.277160] g_ether gadget: g_ether ready [ 3.281372] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 3.287139] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 3.295867] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 3.303039] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 3.310607] usb usb2: Product: MUSB HDRC host driver [ 3.315795] usb usb2: Manufacturer: Linux 2.6.37 musb-hcd [ 3.321472] usb usb2: SerialNumber: musb-hdrc.0 [ 3.328765] hub 2-0:1.0: USB hub found [ 3.332794] hub 2-0:1.0: 1 port detected [ 3.340759] mice: PS/2 mouse device common for all mice [ 3.348968] input: TWL4030 Keypad as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/twl4030_keypad/input/input0 [ 3.366729] ads7846 spi1.0: touchscreen, irq 335 [ 3.373535] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input1 [ 3.387817] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input2 [ 3.402069] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0 [ 3.408935] twl_rtc twl_rtc: Power up reset detected. [ 3.415008] twl_rtc twl_rtc: Enabling TWL-RTC. [ 3.421325] i2c /dev entries driver [ 3.429565] Linux media interface: v0.10 [ 3.434143] Linux video capture interface: v2.00 [ 3.441070] omap3isp supply VDD_CSIPHY1 not found, using dummy regulator [ 3.448181] omap3isp supply VDD_CSIPHY2 not found, using dummy regulator [ 3.455596] omap3isp omap3isp: Revision 15.0 found [ 3.460876] omap-iommu omap-iommu.0: isp: version 1.1 [ 3.533935] mt9t111 2-003c: Unable to detectmt9t111sensor [ 3.544708] isp_register_subdev_group: Unable to register subdev mt9t111 [ 3.553100] tvp514x 3-005c: tvp514x 3-005c decoder driver registered !! [ 3.564056] tvp514x 3-005c: tvp5146m2 (Version - 0x03) found at 0xb8 (OMAP I2C adapter) [ 3.579376] usbcore: registered new interface driver uvcvideo [ 3.585449] USB Video Class driver (v1.0.0) [ 3.590087] omap_device: omap_wdt.-1: new worst case activate latency 0: 30517 [ 3.599151] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec [ 3.605468] omap_device: omap_wdt.-1: new worst case deactivate latency 0: 30517 [ 3.613800] Bluetooth: HCI UART driver ver 2.2 [ 3.618499] Bluetooth: HCI H4 protocol initialized [ 3.623535] Bluetooth: HCILL protocol initialized [ 3.636505] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator [ 3.649383] usbcore: registered new interface driver usbhid [ 3.655273] usbhid: USB HID core driver [ 3.661834] usbcore: registered new interface driver snd-usb-audio [ 3.671966] OMAP3 EVM SoC init [ 3.676849] omap_device: omap_i2c.1: new worst case deactivate latency 0: 61035 [ 3.772003] asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok [ 3.783691] ALSA device list: [ 3.786895] #0: omap3evm [ 3.789703] oprofile: hardware counters not available [ 3.795013] oprofile: using timer interrupt. [ 3.799621] nf_conntrack version 0.5.0 (2621 buckets, 10484 max) [ 3.807250] ip_tables: (C) 2000-2006 Netfilter Core Team [ 3.813354] TCP cubic registered [ 3.816741] Initializing XFRM netlink socket [ 3.821380] NET: Registered protocol family 17 [ 3.826141] NET: Registered protocol family 15 [ 3.831390] Bluetooth: L2CAP ver 2.15 [ 3.835266] Bluetooth: L2CAP socket layer initialized [ 3.840606] Bluetooth: SCO (Voice Link) ver 0.6 [ 3.845367] Bluetooth: SCO socket layer initialized [ 3.850891] Bluetooth: RFCOMM TTY layer initialized [ 3.856018] Bluetooth: RFCOMM socket layer initialized [ 3.861450] Bluetooth: RFCOMM ver 1.11 [ 3.865386] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 3.870941] Bluetooth: BNEP filters: protocol multicast [ 3.876434] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 3.884094] Registering the dns_resolver key type [ 3.889495] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 3.901672] ThumbEE CPU extension supported. [ 3.917602] Power Management for TI OMAP3. [ 3.922515] sr_init: No PMIC hook to init smartreflex [ 3.928253] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized [ 3.936889] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized [ 3.949066] SmartReflex Class3 initialized [ 3.983917] clock: disabling unused clocks to save power [ 3.991394] platform mpu.0: omap_voltage_scale: Already at the requestedrate 1000000000 [ 4.094055] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 4.102844] omap_vout omap_vout: Buffer Size = 3686400 [ 4.121337] omap_vout omap_vout: : registered and initialized video device 16 [ 4.128906] omap_vout omap_vout: Buffer Size = 3686400 [ 4.136077] omap_vout omap_vout: : registered and initialized video device 17 [ 4.147491] Waiting for root device /dev/mmcblk0p2... [ 4.169097] mmc0: new high speed SDHC card at address b368 [ 4.176818] mmcblk0: mmc0:b368 USD 3.75 GiB [ 4.186645] mmcblk0: p1 p2 [ 4.269927] EXT3-fs: barriers not enabled [ 10.545654] kjournald starting. Commit interval 5 seconds [ 10.917144] EXT3-fs (mmcblk0p2): using internal journal [ 10.922698] EXT3-fs (mmcblk0p2): recovery complete [ 10.931701] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 10.939361] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 10.945800] Freeing init memory: 220K INIT: version 2.86 booting Please wait: booting... Starting udev [ 11.718750] udevd (735): /proc/735/oom_adj is deprecated, please use /proc/735/oom_score_adj instead. Remounting root file system... Caching udev devnodes Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory ALSA: Restoring mixer settings... No state is present for card omap3evm Found hardware: "" "" "" "" "" Hardware is initialized using a generic method Configuring network interfaces... No state is present for card omap3evm [ 27.751403] net eth0: SMSC911x/921x identified at 0xd0884000, IRQ: 336 eth0 no wireless extensions. udhcpc (v1.13.2) started Sending discover... Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. Fri Dec 23 00:34:00 UTC 2011 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR [ 41.609100] [ 41.609130] ============================================= [ 41.616302] [ INFO: possible recursive locking detected ] [ 41.621948] 2.6.37 #1 [ 41.624328] --------------------------------------------- [ 41.629943] pvrsrvinit/2142 is trying to acquire lock: [ 41.635314] (psPVRSRVMutex){+.+.+.}, at: [<bf00bbc8>] PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm] [ 41.644561] [ 41.644561] but task is already holding lock: [ 41.650634] (psPVRSRVMutex){+.+.+.}, at: [<bf00eb34>] PVRSRV_BridgeDispatchKM+0x20/0x16c [pvrsrvkm] [ 41.660247] [ 41.660247] other info that might help us debug this: [ 41.667083] 1 lock held by pvrsrvinit/2142: [ 41.671447] #0: (psPVRSRVMutex){+.+.+.}, at: [<bf00eb34>] PVRSRV_BridgeDispatchKM+0x20/0x16c [pvrsrvkm] [ 41.681518] [ 41.681518] stack backtrace: [ 41.686096] [<c004faf0>] (unwind_backtrace+0x0/0xec) from [<c00a91ac>] (__lock_acquire+0xf98/0x18d0) [ 41.695648] [<c00a91ac>] (__lock_acquire+0xf98/0x18d0) from [<c00a9bb8>] (lock_acquire+0xd4/0xf4) [ 41.704925] [<c00a9bb8>] (lock_acquire+0xd4/0xf4) from [<c047375c>] (mutex_lock_nested+0x5c/0x2d8) [ 41.714324] [<c047375c>] (mutex_lock_nested+0x5c/0x2d8) from [<bf00bbc8>] (PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm]) [ 41.725433] [<bf00bbc8>] (PVRMMapRegisterArea+0x14/0x68 [pvrsrvkm]) from [<bf00e944>] (OSAllocPages_Impl+0x68/0xa4 [pvrsrvkm]) [ 41.737426] [<bf00e944>] (OSAllocPages_Impl+0x68/0xa4 [pvrsrvkm]) from [<bf0052e8>] (BM_ImportMemory+0xe4/0x290 [pvrsrvkm]) [ 41.749145] [<bf0052e8>] (BM_ImportMemory+0xe4/0x290 [pvrsrvkm]) from [<bf009b0c>] (RA_Alloc+0xb4/0x288 [pvrsrvkm]) [ 41.760131] [<bf009b0c>] (RA_Alloc+0xb4/0x288 [pvrsrvkm]) from [<bf004cb0>] (BM_Alloc+0xa8/0x280 [pvrsrvkm]) [ 41.770477] [<bf004cb0>] (BM_Alloc+0xa8/0x280 [pvrsrvkm]) from [<bf00aac0>] (AllocDeviceMem+0x80/0x108 [pvrsrvkm]) [ 41.781402] [<bf00aac0>] (AllocDeviceMem+0x80/0x108 [pvrsrvkm]) from [<bf00afd8>] (_PVRSRVAllocDeviceMemKM+0x80/0x158 [pvrsrvkm]) [ 41.793670] [<bf00afd8>] (_PVRSRVAllocDeviceMemKM+0x80/0x158 [pvrsrvkm]) from [<bf015190>] (PVRSRVAllocDeviceMemBW+0x9c/0x1a0 [pvrsrvkm]) [ 41.806701] [<bf015190>] (PVRSRVAllocDeviceMemBW+0x9c/0x1a0 [pvrsrvkm]) from [<bf012d24>] (BridgedDispatchKM+0xd4/0x12c [pvrsrvkm]) [ 41.819152] [<bf012d24>] (BridgedDispatchKM+0xd4/0x12c [pvrsrvkm]) from [<bf00ec28>] (PVRSRV_BridgeDispatchKM+0x114/0x16c [pvrsrvkm]) [ 41.831756] [<bf00ec28>] (PVRSRV_BridgeDispatchKM+0x114/0x16c [pvrsrvkm]) from [<c0116cf8>] (do_vfs_ioctl+0x4e0/0x54c) [ 41.842956] [<c0116cf8>] (do_vfs_ioctl+0x4e0/0x54c) from [<c0116db4>] (sys_ioctl+0x50/0x74) [ 41.851684] [<c0116db4>] (sys_ioctl+0x50/0x74) from [<c0049cc0>] (ret_fast_syscall+0x0/0x3c) [ 41.901855] CMEMK module: built on Dec 22 2011 at 23:52:43 [ 41.907684] Reference Linux version 2.6.37 [ 41.912139] File /datalocal/DVSDK43_HPDL380G7/arago-tmp/work/dm37x-evm-arago-linux-gnueabi/ti-linuxutils-1_2_26_02_05-r102d/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c [ 41.930938] CMEM Range Overlaps Kernel Physical - allowing overlap [ 41.937438] CMEM phys_start (0x83700000) overlaps kernel (0x80000000 -> 0x8b300000) [ 41.946868] allocated heap buffer 0xd2000000 of size 0x2200000 [ 41.953002] heap fallback enabled - will try heap if pool buffer is not available [ 41.960876] cmemk initialized [ 42.061828] DSPLINK Module (1.65.01.05_eng) created on Date: Dec 22 2011 Time: 23:55:34 [ 42.868041] SDMAK module: built on Dec 22 2011 at 23:52:50 [ 42.873870] Reference Linux version 2.6.37 [ 42.878326] File /datalocal/DVSDK43_HPDL380G7/arago-tmp/work/dm37x-evm-arago-linux-gnueabi/ti-linuxutils-1_2_26_02_05-r102d/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/sdma/src/module/sdmak.c numid=49,iface=MIXER,name='HeadsetL Mixer AudioL1' ; type=BOOLEAN,access=rw------,values=1 : values=on numid=46,iface=MIXER,name='HeadsetR Mixer AudioR1' ; type=BOOLEAN,access=rw------,values=1 : values=on Simple mixer control 'Headset',0 Capabilities: pvolume penum Playback channels: Front Left - Front Right Limits: Playback 0 - 3 Mono: Front Left: Playback 1 [33%] [-6.00dB] Front Right: Playback 1 [33%] [-6.00dB] Starting Matrix GUI application. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org dm37x-evm ttyO0 Arago 2011.06 dm37x-evm ttyO0 dm37x-evm login: root root@dm37x-evm:~# /usr/share/ti/ti-dmai-apps/video_loopback_copy_dm3730.x470MV - O lcd -I composite Media: Opened Media Device Enumerating media entities [1]:OMAP3 ISP CCP2 [2]:OMAP3 ISP CCP2 input [3]:OMAP3 ISP CSI2a [4]:OMAP3 ISP CSI2a output [5]:OMAP3 ISP CCDC [6]:OMAP3 ISP CCDC output [7]:OMAP3 ISP preview [8]:OMAP3 ISP preview input [9]:OMAP3 ISP preview output [10]:OMAP3 ISP resizer [11]:OMAP3 ISP resizer input [12]:OMAP3 ISP resizer output [13]:OMAP3 ISP AEWB [14]:OMAP3 ISP AF [15]:OMAP3 ISP histogram [17]:tvp514x 3-005c [17]:tvp514x 3-005c Total number of entities: 17 Enumerating links/pads for entities pads for entity 1=(0 INPUT) (1 OUTPUT) [1:1]===>[5:0] INACTIVE pads for entity 2=(0 OUTPUT) [2:0]===>[1:0] INACTIVE pads for entity 3=(0 INPUT) (1 OUTPU[ 72.254028] tvp514x 3-005c: tvp5146m2 (Version - 0x03) found at 0xb8 (OMAP I2C adapter) T) [3:1]===>[4:0] INACTIVE [3:1]===>[5:0] INACTIVE pads for entity 4=(0 INPUT) pads for entity 5=(0 INPUT) (1 OUTPUT) (2 OUTPUT) [5:1]===>[6:0] INACTIVE [5:2]===>[7:0] INACTIVE [5:1]===>[10:0] INACTIVE [5:2]===>[13:0] ACTIVE [5:2]===>[14:0] ACTIVE [5:2]===>[15:0] ACTIVE pads for entity 6=(0 INPUT) pads for entity 7=(0 INPUT) (1 OUTPUT) [7:1]===>[9:0] INACTIVE [7:1]===>[10:0] INACTIVE pads for entity 8=(0 OUTPUT) [8:0]===>[7:0] INACTIVE pads for entity 9=(0 INPUT) pads for entity 10=(0 INPUT) (1 OUTPUT) [10:1]===>[12:0] INACTIVE pads for entity 11=(0 OUTPUT) [11:0]===>[10:0] INACTIVE pads for entity 12=(0 INPUT) pads for entity 13=(0 INPUT) pads for entity 14=(0 INPUT) pads for entity 15=(0 INPUT) pads for entity 17=(0 OUTPUT) [17:0]===>[5:0] INACTIVE pads for entity 17=(0 OUTPUT) [17:0]===>[5:0] INACTIVE Enabling link [tvp5146]===>[ccdc] [tvp514x]===>[ccdc] enabled Enabling link [ccdc]===>[video_node] [ccdc]===>[video_node] enabled Capture: Current Input: camera VIDIOC_S_INPUT: Invalid argument Capture: Input changed to: camera VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Invalid argument VIDIOC_ENUMSTD: Inval root@dm37x-evm:~#