This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the ti816x output of decode in multiple channel are not in order



All:

 Hi, i input jpeg image 1.jpg,2.jpg,3.jpg,4,jpg,5.jpg  into decode channel: ch_1, ch_2 ,ch_3,ch_4,ch_5 ,

(1.jpg into ch_1,2.jpg into ch_2 .....in the priority order )

but the output order of channel is : ch_5,ch_1,ch_3,ch_2,ch_4 .

does this case is correct ?

i want  the output order is corresponding to input order ,that output order of decode channel is he priority order ch_1,ch_2,ch_3,ch_4,ch_5 in the priority order.

How can i impliment this target ?

  • If frames are fed to different channel they can be output in any order. There is no way to control it. You need some logic in application if you want to order them. Or you can feed all frames to same channel in which case it will be output in order.