This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

selection of arm processor board

sir 

i am participating in texas instruments analog ic design contest 

as part of that i have to list out the components which i am using in it from the 

here i am dealing with nxp lpc2148 arm controller board with two uarts for serial communication compatible with windows7 and an IDE  which can be programmed in C -language 

so can you suggest me the exact part number which can serve the above  requirements and can be exactly replaced in place of nxp lpc2148 arm controller board

along with that i want to know whether TI manufactures GSMmodules  & Heart beat sensor() ? if yes assist me with the part number please thanking you in advance

all the above components are of 0-5 volt range and connected to the micro controller with serial communication like uart 's 

OR IS THERE ANY OTHER DEVELOPMENT BOARD WHICH IS BEST SUITED FOR MY PURPOSE  ALONG WITH  ARM FOR INTERFACING THOSE PERIPHERALS