Hello,
I created an empty project for TMS320DM6437 in CCSv5.
I alos downloaded a linker CMD file (dm6437.cmd) in http://processors.wiki.ti.com/index.php/Linker_CMD_Files_for_CCS#DaVinci.
In the target configuration, I chose EVMDM6437 and "Spectruc Digital XDS560V2.." Connection.
When I run the project, I faced following error messages.
C64XP_0: GEL Output:
EVMDM6437 Startup Sequence
C64XP_0: GEL Output: Setup CacheC64XP_0: GEL Output: (L1P = 32K) +C64XP_0: GEL Output: (L1D = 32K) +C64XP_0: GEL Output: (L2 = ALL SRAM)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output: Setup PinMux...C64XP_0: GEL Output: (Normal operation)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output: Setup Power Modules (All on)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output: Setup PLL1C64XP_0: GEL Output: (DSP = 594 MHz +C64XP_0: GEL Output: SYSCLK2 = 198 MHz +C64XP_0: GEL Output: SYSCLK3 = 99 MHz +C64XP_0: GEL Output: Onchip Oscillator)...C64XP_0: GEL Output: [Already Set]
C64XP_0: GEL Output: Setup PLL2C64XP_0: GEL Output: (VPSS = 54 MHz +C64XP_0: GEL Output: DDR2 Phy = 162 MHz +C64XP_0: GEL Output: Onchip Oscillator)...C64XP_0: GEL Output: [Already Set]
C64XP_0: GEL Output: Setup DDR2 (162 MHz + 32-bit bus)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output: Setup EMIF CS2 - NOR Flash (8-bit bus)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output:
Startup Complete.
C64XP_0: GEL Output: Disable VPSS
C64XP_0: GEL Output: Clear L2 Cache in DDR Range
C64XP_0: GEL Output: Setup CacheC64XP_0: GEL Output: (L1P = 32K) +C64XP_0: GEL Output: (L1D = 32K) +C64XP_0: GEL Output: (L2 = ALL SRAM)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output: Disable EDMA events
C64XP_0: GEL Output: Setup DDR2 (162 MHz + 32-bit bus)...C64XP_0: GEL Output: [Done]
C64XP_0: GEL Output:
C64XP_0: File Loader: Data verification failed at address 0x42000000 Please verify target memory and memory map.
C64XP_0: GEL: File: E:\CS_C6437_Test\test6437\Debug\test6437.out: a data verification error occurred, file load failed.
What is the problem?
Dongseung