Other Parts Discussed in Thread: TMS320DM365
Hello,
I was wondering what is the recommended layout to connect TMS320DM365 RESET and TRST pins?
It is said in the datasheet (p. 206) that:
While both TRST and RESET need to be asserted upon power up, only RESET needs to be released for
the device to boot properly. TRST may be asserted indefinitely for
normal operation, keeping the JTAG port interface and device's
emulation logic in the reset state.
In other words, should I put pull-down or/and pull-up resistors on those net? What if I want to use a button to reset the device?
Thanks,
Mike