Hi,
How can I add metadata to the data going out over VOUT, specifically I want to add a timestamp, aspect ratio flag, frame dimensions and bit rate?
The OMX VFDC is configured to output YUV422 1080p video.
Is there a way to add an additional line in the luminance that could be used for storing metadata?
Can I get access to the buffer to re-write the first line in the luninance as metadata?
Is there a better or simpler option?
Thanks,
Steven