Hi,
Working on SPI Module : SPI 1
1) AM3359 is configured as Master
2) Trying to Communicate with a slave device with frequency 10MHZ API McSPIClkConfig is used and required parameters are passed , But when we use frequency greather than 1MHZ we are not able to transmit data ( Observation in Debug mode : Waits for transmision buffer to be empty).
Below is parameter passed to API McSPIClkConfig
1) baseAdd, : 0x481A0000
2) spiInClk, : 48000000u
3) spiOutClk : 1000000u
4) chNum, : 1
5) clkMode : MCSPI_CLK_MODE_1
Note : For your Information : we were able to successfully communicate with slave device for frequency less than 1MHZ, Communication fails when frequency is increased above 1MHZ
Regards,
Bindu